© Festo SE & Co. KG
2020/06/10
|
ワールドワイド
Mini factories in containers help reduce mask shortages
Protective masks are in short supply in these times of coronavirus so why not just produce some yourself?! With ...
プレスリリースを閲覧する
Protective masks are in short supply in these times of coronavirus so why not just produce some yourself?! With a system from Mikron, this is almost within everyone’s reach. This scalable system produces 50-100 face masks per minute, depending on the version. With engineering support from Festo, Mikron managed to develop the system in just six weeks.
© Mikron
Nils Rödel, Mikron Berlin
Nils Rödel, General Manager of Mikron Berlin.
© Festo SE & Co. KG
CMMT-ST/AS servo drive in Mikron system for mask production
Compatible with higher-level controllers from Beckhoff, Siemens or Rockwell: the servo drive CMMT-ST/AS from Festo.
© Festo SE & Co. KG
DFM guided drive in Mikron system for mask production
Globally and fast available: Products from the Festo core product range like the guided drive DFM shown here preparing the earloops.
© Festo SE & Co. KG
Mikron system for mask production 2
Earloops added and done: Mikron’s scalable system produces 50-100 masks a minute depending on the version.
© Festo SE & Co. KG
Mikron system for mask production 1
Fits in a 20-foot shipping container: Mikron’s system for producing 50-100 protective masks a minute.
© Festo SE & Co. KG
Technology plant VUVG assembly line 2
A compact valve every 12 seconds: automated assembly plants with fast retooling times ensure high output volumes for the automation products of the Festo core product range.
© Festo SE & Co. KG
ELCC-TB cantilever axis with toothed belt
Cantilever axis ELCC-TB for vertical or horizontal operation.