© Festo SE & Co. KG
2024/05/07
|
ワールドワイド
Many functions safe under the roof of VTUX
Festo is now making it even easier for its users: the functions of the classic valve terminals CPV, MPA-L/S and ...
プレスリリースを閲覧する
Festo is now making it even easier for its users: the functions of the classic valve terminals CPV, MPA-L/S and VTUG are now available under the umbrella of the convertible valve terminal VTUX. In addition, the AP-I and AP-A communication system creates the ideal platform for digitalized production. This brings flexibility and openness - true to the motto "Open Architecture".
© Festo SE & Co. KG
VTUX
VTUX: The new valve terminal combines the advantages of three classic valve terminals (photo: Festo)
© Festo SE & Co. KG
Festo Experience Center 2
Festo Experience Center bieten die Möglichkeit, innovativen Kundenservice im Kontext der Digitalisierung voranzutreiben. 
© Festo SE & Co. KG
Valve VHEF
The universal, manual stem actuated valve with pushbutton, switch, hand lever or toggle lever attachment.
© Festo SE & Co. KG
PROFINET bus interfaces from Festo
The new PROFINET bus interfaces from Festo: new features for more applications, including in the process industry.
© Festo SE & Co. KG
Valve terminal CPX-MPA with bus module
Valve terminal CPX-MPA with the new bus module CPX-FB43: Festo has upgraded its PROFINET bus interfaces for the CPX automation platform.
© Festo SE & Co. KG
Valve terminal CPX-VTSA with bus module
Valve terminal CPX-VTSA with the new bus module CPX-FB44/45: Festo has upgraded its PROFINET bus interfaces for the CPX automation platform.
© Festo SE & Co. KG
VUVG assembly line
Festo’s two-step production concept: In the first step, the Global Production Centers produce the basic product components efficiently and in high quantities. This production step is tailored to worldwide demand and does not tend to be linked to...