© Festo SE & Co. KG
Nereda cycle
The Nereda technology is based on a simple cyclical process with three stages, which takes place in one or more Nereda reactors.
© Festo SE & Co. KG
Settling behaviour of Nereda granules
The sedimentation rate of the aerobic, granular biomass is up to thirty times faster in the Nereda process than in conventional plants.
© Festo SE & Co. KG
Nereda plant
The Nereda plant (centre bottom of picture, two large and one smaller round tank) needs more than 75% less space than the conventional plant (centre top of picture, surrounded by trees) while delivering the same purification performance.
© Festo SE & Co. KG
PROFINET bus interfaces from Festo
The new PROFINET bus interfaces from Festo: new features for more applications, including in the process industry.
© Festo SE & Co. KG
Valve terminal CPX-MPA with bus module
Valve terminal CPX-MPA with the new bus module CPX-FB43: Festo has upgraded its PROFINET bus interfaces for the CPX automation platform.
© Festo SE & Co. KG
Valve terminal CPX-VTSA with bus module
Valve terminal CPX-VTSA with the new bus module CPX-FB44/45: Festo has upgraded its PROFINET bus interfaces for the CPX automation platform.
© Festo SE & Co. KG
2021/05/25
|
ワールドワイド
Great strides into the digital future
Digitalisation and artificial intelligence (AI) are mega trends that are also opening up the potential for ...
プレスリリースを閲覧する
Digitalisation and artificial intelligence (AI) are mega trends that are also opening up the potential for savings in all phases of a plant's lifecycle in process automation. A digital field device, the Festo Motion Terminal VTEM, is already available. Festo Dashboards also visualise plant conditions and even artificial intelligence is no longer far removed from becoming a reality in process automation.
© Festo SE & Co. KG
2020/08/07
|
アイルランド, イギリス
Festo Motion Terminal and AI driven Dashboards
Digitalisation and artificial intelligence (AI) are mega trends that are opening up potential savings in ...
プレスリリースを閲覧する
Digitalisation and artificial intelligence (AI) are mega trends that are opening up potential savings in process automation at every phase of a plant's lifecycle. Industrial automation specialist Festo already offers a digital field device, the VTEM Motion Terminal, and Festo Dashboards are available that visualise plant conditions, indicating that AI is becoming a reality in process automation.
© Festo SE & Co. KG
Actuators with decentralised control units
Having the positioner function in a decentralised control unit, in other words not directly at or in the actuator, opens up new horizons right up to the use of artificial intelligence.