© Festo SE & Co. KG
VYKA media-separated solenoid valve
The media-separated solenoid valve VYKA allows the precise dispensing of fluids and the control of liquid flows in manifold duct plates as well as gas flows.
© Festo SE & Co. KG
2024/05/06
|
글로벌, 독일
A real modular DNA factory
Seeds are the new gold. Why is that? Plant-based foods can feed an ever-growing world population. But climate ...
보도 자료 읽기
Seeds are the new gold. Why is that? Plant-based foods can feed an ever-growing world population. But climate change, pests and diseases threaten plant breeding. To help develop resistant seeds and make them available to agriculture, plant breeders need vast amounts of DNA. That is precisely why Synchron Lab has developed the "DNA factory", which is automated with handling gantries, electric axes, pneumatic grippers and sensors from Festo.
© Festo SE & Co. KG
Bert Baas, Festo
Bert Baas, Vertriebsingenieur bei Festo
© Festo SE & Co. KG
Synchron - Glenn Dukel
Glenn Dukel, Project and Business Development Manager at Synchron Lab
© Festo SE & Co. KG
Synchron - intensive washing process
Intensive washing process: in this station, dispense head VTOI dispenses a buffer solution several times to remove salts and ethanol from the DNA.
© Festo SE & Co. KG
Synchron - washing the DNA
Washing the DNA: Here, the magnetic beads and a buffer solution are added to the samples.
© Festo SE & Co. KG
Synchron - from station to station
From station to station: electric axes EGC combined with semi-rotary drive DRRD and a gripper DHPS place the microwell plates on the workpiece carriers of the transport system.
© Festo SE & Co. KG
Synchron - modular DNA factory
With this system 40,000 DNA samples from plants can be extracted fully automatically per day.
© Sens
2023/11/08
|
글로벌, 독일
Ensuring the right pressure
Higher demands on throughput and precision – this is only possible with more automation in laboratory ...
보도 자료 읽기
Higher demands on throughput and precision – this is only possible with more automation in laboratory technology. Sensapex already equips more than 800 customers worldwide with high-precision micromanipulators, microscopes, and pressure controllers – from neuroscience research to in vitro fertilization (IVF) – to name only a few application examples. To work successfully the pressure controllers from Sensapex rely on the decentralized ...
© Festo SE & Co. KG
Sensapex - PGVA-2 pressure and vacuum generator from Festo
For Sensapex, an important component for delivering well controlled and reliable application of pressure is the decentralized pressure and vacuum generator PGVA-2 from Festo.