© Festo SE & Co. KG
BionicBee 2
Natural flight maneuvers with four degrees of freedom: The artificial bee flies with a wingbeat frequency of 15 to 20 hertz. The wings beat forwards and backwards at a 180-degree angle.
© Festo SE & Co. KG
BionicBee 1
The BionicBee is the smallest flying object of the Bionic Learning Network to date. For the first time, the developers used the methodology of generative design.
QM Systems 4
The high-speed vial filling, capping and labelling line designed by QM Systems.
QM Systems 3
A label is printed and applied, giving batch code traceability.    
QM Systems 2
The cap fitting process picks and applies each cap to a specific torque using the Festo EHMD.
QM Systems 1
The automated filling line incorporates Festo’s VTOE dispensing heads and VAEM high speed valve control module.
2024/03/17
|
아일랜드, 영국
New ELGD mechanical axis series from Festo
Machine builders and systems installers are under pressure to deliver high performance automation solutions ...
보도 자료 읽기
Machine builders and systems installers are under pressure to deliver high performance automation solutions that are quicker to deploy and offer a low total cost of ownership. Industrial automation specialist Festo has developed its new ELGD mechanical axis series to meet these demands. Specifically designed for tooth belt and ball screw mechanical axes in cartesian handling systems, the ELGD series features a simplified design that delivers ...
ELGD 2
Cartesian and pick and place solutions for small parts handling are one of many applications that will benefit from the new Festo ELGD axis series.
ELGD 1
Festo’s new ELGD mechanical axis series provide excellent rigidity, large feed forces and high precision in any electro-mechanical automation task and are available in standard and wide profiles.