Op de Next-Gen Life Science Automation onderzoekt Festo nieuwe oplossingen voor medische technologie en laboratoriumautomatisering. Op de Hannover Messe 2026 demonstreren Festo en Fraunhofer IPA de constructie van een cassette voor de processtap van het modificeren van cellen in CAR-T celtherapie. Automatisering vermindert de productietijden en -kosten aanzienlijk, waardoor op maat gemaakte kankertherapieën sneller, goedkoper en voor meer patiënten beschikbaar worden. Persbericht lezen Afbeelding Festo SE & Co. KG 2026/04/15 | Wereldwijd Celtherapieën op maat voor de behandeling van ... Op de Next-Gen Life Science Automation onderzoekt Festo nieuwe oplossingen voor medische technologie ... Persbericht lezen
Festo is expanding its portfolio to include multilayer manifolds made of plastic (bonded manifolds) in order to be able to offer manufacturers of medical and laboratory equipment solutions from a single source. To this end, Festo is taking over the production systems and processes for manufacturing these complex plastic manifolds from Carville, a leading company in this field. Persbericht lezen Afbeelding Festo SE & Co. KG 2024/06/06 | Wereldwijd Festo Expands its Portfolio with Multilayer ... Festo is expanding its portfolio to include multilayer manifolds made of plastic (bonded manifolds) ... Persbericht lezen
Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up new perspectives for pneumatics. Thanks to this technology, the pressure control of the compact proportional valve terminal VTEP is extremely sensitive, down to less than 1 mbar. This is perfect for applications such as wafer polishing or patch clamping in life science. In addition, Controlled Pneumatics uses high-precision piezo valves to reduce compressed air consumption by up to 50%. Persbericht lezen Afbeelding Festo SE & Co. KG 2024/02/05 | Global Pneumatics Makes a Technological Leap with Piezo Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up ... Persbericht lezen
For the gas supply of bioreactors and fermenters or for dosing protective gases - the VEMD mass flow controller from Festo delivers maximum control dynamics and costs significantly less than comparable solutions for the control of air, oxygen and inert gases. Persbericht lezen Afbeelding Festo SE & Co. KG 2023/11/09 | Global Germany A mass flow controller that is silent, fast and ... For the gas supply of bioreactors and fermenters or for dosing protective gases - the VEMD mass ... Persbericht lezen
2024/11/07 | Wereldwijd Compamed 2024 Compamed is the leading exhibition for high-tech solutions in the medical technology sector. Persberichten (9) Afbeeldingen (34) Persmap bekijken Afbeelding Festo SE & Co. KG
2024/04/08 | Global Analytica 2024 April 9th to 12th, 2024 Persberichten (9) Afbeeldingen (34) Persmap bekijken Afbeelding Festo SE & Co. KG
2023/11/08 | Global Compamed 2023 Compamed is the leading exhibition for high-tech solutions in the medical technology sector. Persberichten (9) Afbeeldingen (32) Persmap bekijken Afbeelding Festo SE & Co. KG
2023/02/14 | Global Hannover Messe Press Preview 2023 The future of our planet also presents Festo with major challenges. On the one hand, it is about supplying the world's ... Persberichten (4) Afbeeldingen (23) Persmap bekijken Afbeelding Festo SE & Co. KG