© Wellspect
Wellspect - Energy Efficiency Audit
Part of Wellspect's sustainability strategy: Bo Lilja (on the right side), energy efficiency expert at Festo Sweden, conducts the Energy Efficiency Audit in the presence of Erik Blomholt, Maintenance Engineer at Wellspect (on the left side).
© Wellspect
Wellspect - catheter production
Catheter production at Wellspect: By 2025, Wellspect hopes to have reduced the energy consumption for producing each catheter by 12% compared to 2020.
© Festo SE & Co. KG
2023/02/10
|
Wereldwijd
Saving lives worldwide with low-cost molecular diagnostic tests
Fast MDx shows how many pathogens can be detected with unrivalled speed without the need for expensive ...
Persbericht lezen
Fast MDx shows how many pathogens can be detected with unrivalled speed without the need for expensive biosecure laboratories. This near-patient testing system, developed by London-based company Fast MDx, cuts the typical 24 to 48 hour waiting time to just one to two hours. The new system uses automation technology from Festo.
© Festo SE & Co. KG
Hannes Rößer, Festo
Hannes Rößer, handling technology expert at Festo.
© Festo SE & Co. KG
Fast MDx - operator
After manual placement, operators can focus on their actual task, namely analysing the results.
© Festo SE & Co. KG
Fast MDx - gripping
Fully automated tests: a separate handling system, based on the EXCM-30 planar surface gantry, uses electric griper EHPS-16 to transport and position the microwell plate between the individual processing steps.
© Festo SE & Co. KG
Fast MDx - pipetting 1
Space-saving: one gantry each takes care of pipetting and dispensing liquids as well as transporting and positioning the microwell plate.
© Festo SE & Co. KG
Fast MDx - testing system
High throughput: two 3D gantries with pipetting and transport units ensure a fully automated sequence of molecular diagnostic tests.
© Festo SE & Co. KG
2023/01/25
|
Wereldwijd
Proportional valve technology makes it possible
The sustainability of cardboard packaging is leading to its increasing use instead of plastic packaging. A key ...
Persbericht lezen
The sustainability of cardboard packaging is leading to its increasing use instead of plastic packaging. A key step in the manufacture of folding boxes is the highly precise gluing of the box blanks. The company Baumer hhs is a specialist and global market leader for applications of this type with its dual-piston pump DPP – supported by the proportional valve VPPM from Festo.