© Festo SE & Co. KG
Engineering Tools
The design of a machine lays the foundation of the CO₂ footprint at machine level. Festo supports this first and foremost through free engineering tools.
Energy efficiency audit
© Festo SE & Co. KG
2022/09/28
|
Wereldwijd
How many users of compressed air know where the weak points in their systems ...
Operating costs for pneumatic equipment can be reduced by up to 60% if system operators put into practice the ...
Persbericht lezen
Operating costs for pneumatic equipment can be reduced by up to 60% if system operators put into practice the results and analyses of the Compressed Air Energy Efficiency Audit GFAA by Festo. Energy efficiency experts from Festo use an integrated approach to analyse the entire compressed air system, from the compressor to the application, and recommend measures to reduce energy consumption. Climate protection is also included in the service, since the ...
© Festo SE & Co. KG
Marcus Stemler
Marcus Stemmler, Product Manager Controlled Pneumatics at Festo
piezo technology
© Festo SE & Co. KG
2023/04/17
|
Wereldwijd
Moving into the future with Controlled Pneumatics
The production of tyres and the production of wafers seem to have absolutely nothing to do with each other. In ...
Persbericht lezen
The production of tyres and the production of wafers seem to have absolutely nothing to do with each other. In terms of automation technology, however, they use the same technology: Controlled Pneumatics. That is why Festo has further developed compressed air technology to make pneumatics sustainable, resource-saving and energy-efficient.
© Festo SE & Co. KG
Werner Reichelt
Werner Reichelt, Key Account Manager and Business Development OEM at Festo
© Festo SE & Co. KG
Christian Burdin
Christian Burdin, Sales Operations Service and Support at Festo
artificial intelligence
© Festo SE & Co. KG
2022/09/28
|
Wereldwijd
Identifying waste with artificial intelligence
High energy prices, increasing cost pressure and the goal of climate-neutral production have pushed energy ...
Persbericht lezen
High energy prices, increasing cost pressure and the goal of climate-neutral production have pushed energy efficiency to the top of the agenda in many companies. Festo Energy Saving Services to DIN EN ISO 11011 offer a customised range of services to provide support with this topic. As part of these services, energy efficiency experts from Festo work with customers and users to identify potential savings in how compressed air is used ...
© Festo SE & Co. KG
Rebecca Sacher
Rebecca Sacher, Project manager for CO₂ reduction in Sales at Festo
Engineering tools
© Festo SE & Co. KG
2022/09/28
|
Wereldwijd
Reducing CO₂ through sustainable engineering
When it comes to reducing product-related CO₂ emissions, Festo can leverage two important aspects and also ...
Persbericht lezen
When it comes to reducing product-related CO₂ emissions, Festo can leverage two important aspects and also focuses on an all-encompassing approach to the CO₂ emissions caused by its products. The design of a machine lays the foundation of the CO₂ footprint at machine level. Festo supports this process first and foremost through free engineering tools. In addition, the key to a carbon-neutral future is to look at and assess ...