© Festo SE & Co. KG
HAHN Automation Group - End-of-line test system
All relevant test scenarios for 90% of all battery packs available on the market can be implemented on the end-of-line test system.
© Festo SE & Co. KG
HAHN Automation Group - Battery tester EOLT
Fully automated 100% testing of battery cells: with the EOLT battery tester from HAHN Automation Group  
© Festo SE & Co. KG
2023/03/16
|
Wereldwijd
Optimising curing presses with AI
Digitalisation and artificial intelligence (AI) are megatrends that can also offer great potential for savings ...
Persbericht lezen
Digitalisation and artificial intelligence (AI) are megatrends that can also offer great potential for savings in tyre production. Machine learning algorithms can be implemented in a decentralised manner, for example on the edge, i.e. on the actual module to be monitored. An example is Festo AX. This AI software uses these algorithms to detect anomalies on tyre building machines or in curing presses.
© Festo SE & Co. KG
Health Monitoring Tire Curing
Digitalisation and artificial intelligence (AI) are megatrends that can also offer great potential for savings in tyre production. An example is Festo AX. This AI software uses these algorithms to detect anomalies on tyre building machines or in...
Battery Pack Handling
© Festo SE & Co. KG
2023/05/15
|
Wereldwijd
From battery cell production to the installation of electric motors
The number of vehicles with electric powertrains is growing globally by more than 40% each year. At the same ...
Persbericht lezen
The number of vehicles with electric powertrains is growing globally by more than 40% each year. At the same time, the manufacturing processes for the electrified powertrain are changing. While the classic manufacturing process for cars with internal combustion engines was predominantly based on semi-automatic production methods, both battery cells and electric motors are increasingly produced fully automatically. As a leading manufacturer of ...
Battery Pack Handling
© Festo SE & Co. KG
Battery Pack Handling
Handling solutions that have a mix of electric and pneumatic components offer the combined benefits of both technologies and ensure the sturdy, reliable and precise gripping and transporting of battery cells. In this handling system for battery...