How many users of compressed air know where the weak points in their systems ...
Operating costs for pneumatic equipment can be reduced by up to 60% if system operators put into practice the ...
Czytaj informację prasową
Operating costs for pneumatic equipment can be reduced by up to 60% if system operators put into practice the results and analyses of the Compressed Air Energy Efficiency Audit GFAA by Festo. Energy efficiency experts from Festo use an integrated approach to analyse the entire compressed air system, from the compressor to the application, and recommend measures to reduce energy consumption. Climate protection is also included in the service, since the ...