© Festo SE & Co. KG
Application Festo Motion Terminal VTEM pick & place
Highly flexible pick & place: the Festo Motion Terminal positions using pneumatics.
© Festo SE & Co. KG
2020/11/26
|
Świat
Ideal for automation in the chemical industry
The quarter turn actuator DFPD-C from Festo is well equipped for the harsh conditions in the chemical industry. ...
Czytaj informację prasową
The quarter turn actuator DFPD-C from Festo is well equipped for the harsh conditions in the chemical industry. It is suitable for actuating butterfly valves, globe valves and ball valves in process plants in the chemical and petrochemical industry and can also be used with a positioner for control applications.
© Festo SE & Co. KG
DFPD-C-VDE2 quarter turn actuator with manifold block
Quarter turn actuator DFPD-C-VDE2 with manifold block and NAMUR Interface.
© Festo SE & Co. KG
DFPD-C quarter turn actuator
Equipped for the harsh conditions in the chemical and petrochemical industry: the quarter turn actuator DFPD-C from Festo.
Polish translation unavailable for KI Erfolgsstory Resolto.
Agitazione, movimenti improvvisi della bocca: il robot umanoide simula il possibile comportamento dei bambini durante un trattamento dentale.
© tmsuk, Japan
2023/03/13
|
Świat
No longer afraid of the dentist
No one enjoys going to the dentist; young children even less so. To help future dentists and dental assistants ...
Czytaj informację prasową
No one enjoys going to the dentist; young children even less so. To help future dentists and dental assistants deal with children during dental treatments, the Japanese company tmsuk has developed a humanoid robot that realistically simulates the behaviour of young children during these treatments, complete with fidgeting, flinching or closing the mouth. The dummy’s realistic movements are produced using proportional pressure regulators with ...
© Festo SE & Co. KG
VEAA/VEAB proportional pressure regulator
Silent, smooth and fast thanks to piezo technology: the VEAA/VEAB proportional pressure regulator.
Agitazione, movimenti improvvisi della bocca: il robot umanoide simula il possibile comportamento dei bambini durante un trattamento dentale.
© tmsuk, Japan
Pedia Roid Simulation of dental treatment 2
Fidgeting, twitching or sudden closing of the mouth: The humanoid robot for training purposes simulates the possible behaviour of children during a dental treatment.
© tmsuk, Japan
Pedia Roid Simulation of dental treatment 1
The Pedia Roid robot for training dentists and dental assistants: Piezo technology simulates lifelike movements.
Festo Pressebild Syria
© Festo SE & Co. KG
Lecture in one of the newly equipped laboratories at the University of Damascus