© Festo SE & Co. KG
SupraSensor_1
The SupraSensor exhibit demonstrates the function of a contactless balance, which could be used for example on sterile workbenches in biological or chemical analytics.
© Festo SE & Co. KG
VZQA
The pinch valve VZQA: flexible connection options.
© Festo SE & Co. KG
NPCK
Fulfilling all the Clean Design requirements: the stainless steel fitting NPCK.
© Festo SE & Co. KG
ESBF
The electric cylinder ESBF from Festo in Clean Look is perfect for positioning in critical areas of production lines.
© Festo SE & Co. KG
CRDSNU
Saving time with the self-adjusting cushioning PPS and the enhanced ease of cleaning of the round cylinder CRDSNU in Clean Design.
© Festo SE & Co. KG
MPA-C Valve Terminal 2
IP69K and Clean Design:  the valve terminal MPA-C.
© Festo SE & Co. KG
MPA-C Valve Terminal 1
Setting a high standard: the Clean Design valve terminal MPA-C meets the requirements for protection class IP69K and CRC4, the highest corrosion resistance class at Festo.
© Festo SE & Co. KG
YXMx
Kinematics with controller, software packages for motion tasks and condition monitoring, and an app for cloud-based visualisation: the Compact Handling System YXMx from Festo.
© Festo SE & Co. KG
VTEM Motion Terminal 3
Multi-Carrier-System®: Das flexible modulare Transportsystem lässt sich auf Knopfdruck via Software an unterschiedliche Formate anpassen.
© Festo SE & Co. KG
VTEM Motion Terminal 2
With the Festo Motion Terminal, pneumatic functions can be controlled via apps for the first time, without having to change or modify the hardware.