2007/04/01
Air_ray
© Festo SE & Co. KG
2021/11/15
|
Global
The right handling system in a matter of minutes
With the Handling Guide Online, design engineers can create the right ready-to-install handling system from ...
Ler comunicados de imprensa
With the Handling Guide Online, design engineers can create the right ready-to-install handling system from Festo in record time, whether for a 2D linear and planar surface gantry, a 3D gantry or a new 3D cantilever system. Not only can they now plan extremely compact or extremely dynamic Cartesian robots using the intuitive configuration and ordering software, but they also benefit from the circuit diagram service from Eplan and commissioning files.
© Festo SE & Co. KG
Handling Guide Online
With the Handling Guide Online, machine and system builders are able to reduce their time to market for integrated handling systems by up to 70%.
© Festo SE & Co. KG
FinRay Gripper
The FinRay gripper from Festo offers gripper fingers that adapt to the workpiece. This allows safe and tactile gripping of workpieces with plastic malleability such as pouch cells.
© Festo SE & Co. KG
CPX-AP-I
The remote IO system CPX-AP-I seamlessly integrates all IOs and IO-Link participants such as sensors and valve terminals into the communication network of the plant. This ensures seamless communication from the workpiece to the cloud.
© Festo SE & Co. KG
Cantilever handling system spindle axes ELGT
A cantilever handling system based on spindle axes ELGT ensures dynamic and safe loading and unloading of the process chamber.
© Festo SE & Co. KG
Degassing process chambers
The core of the application is the process chamber. Pneumatic and electric actuators manipulate hollow lances and pierce the battery cells.
© Festo SE & Co. KG
2023/05/15
|
Global
Reliable degassing in battery cell production
Degassing and sealing are core processes in battery cell production that directly follow the initial contacting ...
Ler comunicados de imprensa
Degassing and sealing are core processes in battery cell production that directly follow the initial contacting of the battery cells with electrical voltage. The battery cells are pierced with lances and the forming gas produced during contacting is extracted. Pneumatic and electric actuators from Festo are used to handle and pierce the battery cells.
© Festo SE & Co. KG
Martin Stadler, ViscoTec
Martin Stadler, Managing Director of ViscoTec
© Festo SE & Co. KG
Christian Heidinger, ViscoTec
Christian Heidinger, Head of Product Management at ViscoTec