© Festo SE & Co. KG
WorldSkills Competition Industry 4.0
Heads are spinning: Scene from the Industry 4.0 competition at WorldSkills
© Festo SE & Co. KG
WorldSkills Opening Ceremony
Just like the Olympics: atmosphere at the opening ceremony of the WorldSkills vocational world championships
© Festo SE & Co. KG
2024/09/05
|
Global
After the Olympics in Paris, now the WorldSkills in Lyon
The Olympic Games in Paris are over – now another French metropolis is taking center stage: Lyon will ...
Ler comunicados de imprensa
The Olympic Games in Paris are over – now another French metropolis is taking center stage: Lyon will host the 47th WorldSkills from September 10 to 15, 2024. The WorldSkills Championships will bring together more than 1,500 young people from over 65 countries and regions to compete in 62 competitions.
© Festo SE & Co. KG
2024/06/06
|
Global
Festo Expands its Portfolio with Multilayer Manifolds
Festo is expanding its portfolio to include multilayer manifolds made of plastic (bonded manifolds) in order to ...
Ler comunicados de imprensa
Festo is expanding its portfolio to include multilayer manifolds made of plastic (bonded manifolds) in order to be able to offer manufacturers of medical and laboratory equipment solutions from a single source. To this end, Festo is taking over the production systems and processes for manufacturing these complex plastic manifolds from Carville, a leading company in this field.
© Festo SE & Co. KG
Multilayer Manifold
Multilayer manifolds for manufacturers of medical and laboratory equipment: in future, Festo will offer these in combination with media-separated valves from a single source. 
© Festo SE & Co. KG
Battery Recycling
Recovering valuable lithium, cobalt, manganese and nickel from used batteries and reuse them for the production of new batteries: Automated recycling processes enable these rare minerals to be reused economically and cleanly. Festo has the right...
© Festo SE & Co. KG
Festo SupraMotion 2024: Levitation Gap
The magnetic forces between the superconductor and the carrier on which the containers are transported allow levitation heights of 10 millimeters and more.
© Festo SE & Co. KG
Festo SupraMotion 2024: Filling
Two VTOE dosing heads fill the container with liquid.