© Festo SE & Co. KG
Piezoelectric valves
Controlled Pneumatics proportional pressure regulators feature piezoelectric valves, a technology Festo has been applying for decades and now mass produces.
© Festo SE & Co. KG
Controlled Pneumatics
Controlled Pneumatics features closed-loop control of proportional pressure regulators and delivers energy efficiency, high dynamics, and precision motion.
© Festo SE & Co. KG
2025/02/06
|
Canada, EUA
Festo Introduces the VEFC Mass Flow Controller for Precise Control of Inert ...
Festo introduces the VEFC mass flow controller, the company’s latest entry into its Controlled Pneumatics ...
Ler comunicados de imprensa
Festo introduces the VEFC mass flow controller, the company’s latest entry into its Controlled Pneumatics family of solutions. The VEFC features precisely controlled flow of inert gases of up to 200 l/min and is one of the most compact mass flow controllers on the market – only 24 mm wide. Like all Controlled Pneumatics solutions, the VEFC features energy efficient piezoelectric valve technology integrated with control algorithms and ...
VEFC
Once a setpoint is set, the Festo VEFC mass flow controller maintains it without hysteresis. The VEFC delivers up to 200 l/min flow and is one of the most compact units on the market.
© Festo SE & Co. KG
2025/01/15
|
Canada, EUA
Festo Introduces the VTUX, the Company’s new Flagship Valve Terminal
Festo introduces its new flagship valve terminal, the VTUX. The VTUX can serve as I/O, remote I/O, and ...
Ler comunicados de imprensa
Festo introduces its new flagship valve terminal, the VTUX. The VTUX can serve as I/O, remote I/O, and decentralized I/O. These compact and rugged IP65/67-rated terminals can be located anywhere on a machine that boosts operational performance and original equipment manufacturer (OEM) installation productivity. VTUX modularity results in less inventory and lower overhead costs. Slated to replace Festo’s legacy terminals, the VTUX will be the ...
© Festo SE & Co. KG
VTUX
The VTUX valve terminal assembled as remote I/O with the CPX-AP-A communications module, left, I/O, center, and two subbases with a total of eight valve slices, right. Each terminal can have up to 128 valves.
© Festo SE & Co. KG
Individual polishing chambers
The variable contact pressure of the individual polishing chambers is controlled precisely using VTEP. This ensures excellent results, even when polishing wafers.
© Festo SE & Co. KG
Best control for dancer rollers
The VTEP provides the best control for dancer rollers in web tensioning applications.
© Festo SE & Co. KG
Target reached
The “motion complete” function, familiar from electric drive technology, is now also available for pneumatic pressure control as “target reached.”