© Festo SE & Co. KG
Nereda cycle
The Nereda technology is based on a simple cyclical process with three stages, which takes place in one or more Nereda reactors.
© Festo SE & Co. KG
Settling behaviour of Nereda granules
The sedimentation rate of the aerobic, granular biomass is up to thirty times faster in the Nereda process than in conventional plants.
© Festo SE & Co. KG
Nereda plant
The Nereda plant (centre bottom of picture, two large and one smaller round tank) needs more than 75% less space than the conventional plant (centre top of picture, surrounded by trees) while delivering the same purification performance.
© Festo SE & Co. KG
CPX automation platform
Integrates the entire electropneumatic control chain: the CPX automation platform.
© Festo SE & Co. KG
Automation of modular plants
Automation of modular plants: highly flexible and modular production plants with decentralised automation enable the process industry to react to fluctuations in demand.
© Festo SE & Co. KG
2021/05/24
|
Global
Simplified integration into control systems
Highly flexible and modular production plants with decentralised automation enable the process industry to ...
Ler comunicados de imprensa
Highly flexible and modular production plants with decentralised automation enable the process industry to react to fluctuations in demand. This is the case in water treatment, in the pharmaceutical, fine chemical and food industries and also in energy generation. Decentralised controllers from Festo are perfect for this. Festo developed the PA-Toolkit for programming these controllers to enable simple application engineering in line with the ...
© Festo SE & Co. KG
PA-Toolkit
The PA-Toolkit from Festo for programming decentralised controllers enables simple application engineering in line with MTP from Namur and ZVEI.