© Festo SE & Co. KG
Sensapex - VEAB proportional pressure regulator from Festo
Sensapex uses up to eight piezo-based proportional pressure regulators VEAB from Festo in their uMc pressure controllers.
© Sens
Sensapex - complete system
A complete solution for higher throughput and accuracy in lab automation – including microscopes and pressure controllers from Sensapex as well as the pressure and vacuum generator PGVA-2 from Festo.
© Festo SE & Co. KG
Sensapex - uMc pressure controllers
Higher throughput and accuracy: lab automation with uMc pressure controllers from Sensapex relying on piezo-based pressure regulators VEAB from Festo.
© Festo SE & Co. KG
Festo Experience Center 2
Festo Experience Center bieten die Möglichkeit, innovativen Kundenservice im Kontext der Digitalisierung voranzutreiben. 
© Festo SE & Co. KG
2023/07/19
|
EUA
Festo Brings Automated Sample and Liquid Handling Solutions to AACC 2023
Festo features at AACC 2023 Cartesian gantry systems for handling samples and a flexible, high accuracy liquid ...
Ler comunicados de imprensa
Festo features at AACC 2023 Cartesian gantry systems for handling samples and a flexible, high accuracy liquid dispensing system, that enables manufacturers to reduce engineering and procurement overhead while speeding time to market. (Festo AACC [American Association for Clinical Chemistry] Booth #4457, July 23-27, Anaheim Convention Center, Anaheim, Calif.)
© Festo SE & Co. KG
2023/08/04
|
Canada
Saving lives with low-cost molecular diagnostic tests, with Festo on board
The Fast MDx testing system is not only a game-changer in pathogen detection, it promises to be a life saver. ...
Ler comunicados de imprensa
The Fast MDx testing system is not only a game-changer in pathogen detection, it promises to be a life saver. Available starting in June, Fast MDx is the world’s first fully automated, high-throughput, near-patient molecular diagnostic testing system.  Developed by the London, England-based social enterprise company of the same name with engineering support and automation technology from Festo, this extremely compact, mobile platform cuts ...
© Festo SE & Co. KG
Syntegon - EHPS electric standard gripper from Festo
The electric parallel gripper EHPS from Festo also contributes to the flexibility of the Elematic 3001 WAH case packer by reliably adapting the gripping force to sensitive workpieces.
© Festo SE & Co. KG
2024/05/06
|
Global
Extremely high sample throughput rates
If there’s one thing the corona pandemic has taught us, it is that laboratories place tremendous ...
Ler comunicados de imprensa
If there’s one thing the corona pandemic has taught us, it is that laboratories place tremendous importance on high sample throughput rates. Even with highly qualified laboratory personnel, this demand can no longer be met. There’s no getting round the automation of laboratory processes. That’s why MolGen in the Netherlands developed PurePrep TTR, which can prepare 320 patient samples per hour for molecular downstream processing. And ...
© Festo SE & Co. KG
DHOE pipetting head
An open pipetting system with pipetting head DHOE for simple liquid transport makes it possible to configure the most important pipetting functions based on requirements, and to expand them flexibly – the system is also compatible with the largest...