© Festo SE & Co. KG
BEC – Servo drive CMMT-ST
Practical: the drive amplifiers, in this case the servo drives CMMT-ST, are mounted on the robot itself, rather than on the gripper system. This frees up space on the gripper and makes it less complicated.
© Festo SE & Co. KG
BEC – Supports with electric cylinders
Flexible, robust and precise: the supports with electric cylinders from Festo need to be powerful enough to be able to hold the coils weighing up to 1.5 tonnes, but at the same time not so powerful that they damage them.
© Festo SE & Co. KG
BEC – High-tech gripper system
High-tech gripper system on the articulated arm robot. It is vital that the coils do not twist or slip when the gripper picks them up and inserts them into the magnets; the tolerance for inserting the coils into the magnets is no more than 0.5...
© Festo SE & Co. KG
BEC – Insertion of coils into the magnets
Collaborative solution: coils weighing several tonnes are inserted precisely into the magnets of magnetic resonance imaging machines.
© Festo SE & Co. KG
Aspirating
Fast and reliable aspiration: the dispense head VTOI controls all eight channels with just one valve.
© Festo SE & Co. KG
Pipetting
Reliable pipetting results: intelligent pipette head DHOP set up with the finely tuned disposable tips DHAP.
© Festo SE & Co. KG
2022/06/15
|
Global
Smart pipetting for safe laboratory processes
Handling the smallest amounts of liquids down to the microlitre range requires high levels of precision and ...
Ler comunicados de imprensa
Handling the smallest amounts of liquids down to the microlitre range requires high levels of precision and flexibility because of the changing fluid properties of the different media. Pressure-controlled liquid handling systems enable precise, scalable liquid handling. Festo has suitable solutions for these systems, whether for pipetting, dispensing or aspirating. Individual modules are available, such as the smart pipette head DHOP, but as well the ...
© Festo SE & Co. KG
Miniature valve VOVK
Compact components: The miniature valves VOVK activate the process which ensures that the liquid reagents react with each other and the analysis process starts.
© Festo SE & Co. KG
Key Visual LifeTech
Components and automation solutions for laboratory automation and medical technology
© Festo SE & Co. KG
DHOP pipetting head
The smart DHOP pipetting head impresses with its intuitive operation and easy setting of the target volume.