© Festo SE & Co. KG
VPWS proportional valve
Safe and precise control of gases with the proportional valve VPWS from Festo.
© Festo SE & Co. KG
Niels Kruize
Niels Kruize, Business Development, Synchron Lab Automation.
© Festo SE & Co. KG
CPX-E Synchron 2
CPX-E and valve terminals VTUG with IO-Link control the system.
© Festo SE & Co. KG
EGC Synchron
Electric axes EGC in combination with an electric slide EGSL position the pipetting head for DNA extraction.  
© Festo SE & Co. KG
EGSC Synchron
An electric slide EGSC moves the pipetting head down to add liquid to the microwell plates at several washing stations.
© Festo SE & Co. KG
Planar surface gantry for laboratory automation
The best possible solution for system manufacturers: as well as its own components such as the planar surface gantry EXCM, Festo also integrates components from third-party manufacturers.
© Festo SE & Co. KG
VAEM
The VAEM valve control module with holding current reduction is ideal for controlling dosing heads.  
© Festo SE & Co. KG
VTOE
Contactless dispensing of very small volumes: the 8-channel dispense head VTOE is a configurable complete solution comprising manifold duct plate, dosing valves and nozzles.
© Festo SE & Co. KG
Valve block for the point-of-care application
Based on the layout of the microfluidic chip, Festo develops the appropriate valve block for the point-of-care application.
© Festo SE & Co. KG
Festo LifeTech
Mobile analytical devices allow fast testing to identify pathogens in the case of colds or flu-like infections as well as other bacterial or viral diseases.