© Festo SE & Co. KG 2024/06/06 | Globale Festo Expands its Portfolio with Multilayer Manifolds Festo is expanding its portfolio to include multilayer manifolds made of plastic (bonded manifolds) in order to ... Lire le communiqué de presse Festo is expanding its portfolio to include multilayer manifolds made of plastic (bonded manifolds) in order to be able to offer manufacturers of medical and laboratory equipment solutions from a single source. To this end, Festo is taking over the production systems and processes for manufacturing these complex plastic manifolds from Carville, a leading company in this field.
© Festo SE & Co. KG 2024/04/23 | Globale Superconductor technology: Contactless working in the laboratory of the future Superconductor technology enables the contactless movement and handling of objects – ideal for ... Lire le communiqué de presse Superconductor technology enables the contactless movement and handling of objects – ideal for high-tech industries such as laboratory automation or biotechnology. At the Hannover Messe, Festo presents a concept for the fully automated filling and weighing of freeze-dry containers in cleanrooms. Thanks to SupraMotion levitation modules and products from the Festo automation portfolio for laboratory applications, the highest standards of ...
© Festo SE & Co. KG 2024/05/07 | Globale Biologization Makes Ecological Innovations Possible for the World of Tomorrow Festo presented a unique concept for the simple storage and safe transportation of hydrogen using bacteria ... Lire le communiqué de presse Festo presented a unique concept for the simple storage and safe transportation of hydrogen using bacteria with its “BionicHydrogenBattery” exhibit in 2024. The company also demonstrated how industrial bioprocesses can be operated efficiently in the long-term using a wide range of components and solutions from the Festo product portfolio. Festo is also committed to biologization as a field of learning: with modular learning ...
© Festo SE & Co. KG 2024/05/06 | Globale Automated nitrogen analysis reduces costs per sample The world's population is growing and with it the demand for food and animal feed with clearly verifiable ... Lire le communiqué de presse The world's population is growing and with it the demand for food and animal feed with clearly verifiable ingredients. This includes the protein content. This can be determined by nitrogen analysis – fully automaticated with the new N-Realyzer from C. Gerhardt. The laboratory system ensures high throughput, is low-maintenance and intuitive to operate. Among other things, it owes this to a valve block from Festo, which offers high tightness in ...
2024/06/06 | Globale Achema 2024 Communiqués de presse (8) Illustrations (24) Vidéos (0) Voir le dossier de presse © Festo SE & Co. KG
2024/05/28 | Globale Battery Show Europe 2024 Reliable, economical, sustainable: The circular battery life cycle – solutions from cell production ... Communiqués de presse (0) Illustrations (0) Vidéos (0) Voir le dossier de presse © Festo SE & Co. KG
2024/05/07 | Globale Hannover Messe 2024 Progress in motion: How do we meet the great challenges of our time? Supplying the world's population ... Communiqués de presse (11) Illustrations (37) Vidéos (0) Voir le dossier de presse © Festo SE & Co. KG
2024/05/06 | Globale Analytica 2024 April 9th to 12th, 2024 Communiqués de presse (9) Illustrations (34) Vidéos (0) Voir le dossier de presse © Festo SE & Co. KG