2024/05/07
ID: 4773

Biologization Makes Ecological Innovations Possible for the World of Tomorrow

From algae cultivation, hydrogen storage and transportation to educational concepts

Festo presented a unique concept for the simple storage and safe transportation of hydrogen using bacteria with its “BionicHydrogenBattery” exhibit in 2024. The company also demonstrated how industrial bioprocesses can be operated efficiently in the long-term using a wide range of components and solutions from the Festo product portfolio. Festo is also committed to biologization as a field of learning: with modular learning systems, an additional Chamber of Commerce qualification and the development of a “Biomechatronics” degree course.

With its automation technology, Festo aims to provide climate-friendly solutions and thereby contribute to improving the quality of life of present and future generations. For this reason, the company is working intensively on how processes can be carried out with less material consumption and more recycling, and which alternative materials can be used. Developing biology as a field of activity for automation is particularly promising. The smallest factory of the future will be found in a biological cell.

With automation technology, biological processes that take a long time in nature can be accelerated, scaled up and made economically viable as a result. Thanks to a combination of many years of experience and highly developed technology, Festo plays a leading role, demonstrating what is possible with automation and sophisticated control and regulation technology in the field of biologization. Following its “PhotoBionicCell” (2022) and “BionicCellFactory” (2023) bioreactors, which focused on the cultivation of algae, Festo's current “BionicHydrogenBattery” project deals with one of the energy sources of tomorrow: hydrogen.

BionicHydrogenBattery – safe storage and transportation of hydrogen with the help of bacteria

As things stand at present, hydrogen can only be stored and transported safely and in a space-saving manner using processes that require extremely high or low temperatures and high pressures of 150-700 bar, which requires a lot of energy. With the fully automated biotechnological system “BionicHydrogenBattery”, Festo is presenting a completely new approach: the volatile substance is converted into formic acid with the help of bacteria in a low-risk and energy-efficient manner – and at comparatively low temperatures of around 65 °C and a low pressure of 1.5 bar. The acid can be easily stored and transported. At the destination, the same bacteria reverse the process and decompose the acid back into CO2 and hydrogen. While the latter can be used to generate electricity, the high-purity CO2 could be recycled and used in the beverage industry, for example. In the exhibit, it is recycled within the scope of a circular economy and reused to produce formic acid. 

The core of the biological process is the bacterium Thermoanaerobacter kivui (T. kivui). These bacteria have a special enzyme that enables them to convert hydrogen and CO2 into formic acid. This process was discovered and fundamentally researched by the team led by Prof. Dr. Volker Müller, head of the Molecular Microbiology and Bioenergetics department at Goethe University Frankfurt, with whom the Festo team is working closely on the project. “Hydrogen is one of the energy sources of the future, which will play an important role in the generation of clean electricity, among other things,” says Dr. Michael Sinsbeck, Head of Bionic Projects at Festo. “With our concept, we are helping to make this potential economically viable.”

BioTech Automation: Reactors for algae and bacteria

Bioprocesses are becoming increasingly important for the industry as they offer sustainable alternatives to conventionally manufactured products. “In addition to algae, we can also use many other organisms that produce food, biofuel or bioplastics from renewable resources, for example,” says Dr. Elias Knubben, Head of Research and Innovation at Festo. Festo therefore presented an overview of the components and solutions already available at the Hannover Messe using selected cultivation processes, which will be demonstrated in two bioreactors: an algae reactor (FPA, Subitec) using the example of Chlorella vulgaris and a stainless-steel reactor for the cultivation of micro-organisms such as E. coli.

“With our product portfolio, we can already serve the growing biologization market in many areas, particularly in gassing, liquid handling and the holistic automation of bioreactors,” says Ralf Kapfhamer, Advanced Development Biotech and Process Automation. A key product here is the new VTUX valve terminal, which enables the pneumatic valves on bioreactors to be controlled.

 In addition to individual components, Festo also offers customized system solutions for bioreactors. Customized automation solutions are developed from selected components, for example, in the form of complete control cabinets. Customer-specific software can also be created, from the control system to the cloud. Seamless integration of the systems and the ability to analyze data in real time enable efficient and transparent process control.

Biologization as a field of learning: new training module and degree course  

The operation of a bioprocess requires knowledge from the fields of electrical engineering, mechanics, computer science and biotechnology. A new job profile is emerging: the biomechatronics technician. In a modular learning concept, the learning reactor, this knowledge is taught using a combination of hardware and software.

Festo is not only meeting the new challenges in the field of biologization from a technical perspective, but as a market leader in technical and further education, it is also keeping an eye on the qualifications required in the future. In the area of its own vocational training, Festo has therefore launched the additional qualification "Climate protection and sustainable development" together with the Stuttgart Region Chamber of Industry and Commerce. It is aimed at many training professions. There will be an "Automation of Biological Transformation" module for industrial-technical and commercial trainees in particular. Festo will cover parts of this topic in its training center, starting with its own trainees. Festo is also developing a modular learning concept for prospective biomechatronics engineers, which can be used to impart knowledge, especially technical basics.

Festo also has concrete plans for higher education: “We are training the specialists of the future, which is why we are currently working with Reutlingen University to design a new biomechatronics course that combines biological and technical content with a focus on the cell as the world's smallest factory,” says Stefan Dietl, Head of Training at Festo. “The students will primarily be able to learn technical skills with us.” The new learning reactor will also be used here. 

Festo est à la fois un acteur mondial et une entreprise familiale indépendante basée à Esslingen am Neckar en Allemagne. Depuis ses débuts, Festo établit des normes en matière de technologie d'automatisation industrielle et de formation technique, contribuant ainsi au développement durable de l'environnement, de l'économie et de la société. La société fournit une technologie d'automatisation pneumatique et électrique à 300 000 clients d'automatisation d'usine et de processus dans plus de 35 industries. Le secteur LifeTech, avec la technologie médicale et l'automatisation des laboratoires, devient de plus en plus important. Les produits et services sont disponibles dans 176 pays du monde. Dans le monde entier, environ 20 600 employés dans environ 60 pays avec plus de 250 succursales ont généré un chiffre d'affaires d'environ 3,45 milliards d'euros en 2024. Sur ce total, plus de 8 % sont investis chaque année dans la recherche et le développement. Dans l'entreprise apprenante, les mesures de formation et de développement représentent 1,5 % du chiffre d'affaires. Festo Didactic SE est l'un des principaux fournisseurs d'enseignement et de formation techniques et propose à ses clients du monde entier des solutions complètes d'apprentissage numérique et physique dans l'environnement industriel.

© Festo SE & Co. KG
BionicHydrogenBattery
With the biotechnological system BionicHydrogenBattery, Festo is presenting a completely new solution for the storage of hydrogen. It is converted into formic acid with the help of bacteria – energy-efficient and with a low risk.
© Festo SE & Co. KG
BionicHydrogenBattery: cultivation reactor
In the cultivation reactor the bacteria T. kivui grow under optimized conditions, thanks to automation technology.
© Festo SE & Co. KG
BionicHydrogenBattery: engineering
Biologization means: not only do we learn from nature, but also work with it. In this way, we enable ecological innovations for the world of tomorrow.
© Festo SE & Co. KG
BioTech Automation
BioTech Automation: Festo will be presenting an overview of components and solutions already available for the automation of bioreactors based on selected cultivation processes.
© Festo SE & Co. KG
BioTech Automation: Algae reactor
Products from the areas of gas handling, liquid handling and control technology are used in the algae reactor.
© Festo SE & Co. KG
BioTech Automation: Bioreactor
The stainless steel reactor is an example for the cultivation of microorganisms such as E. coli with components from the Festo product portfolio.
© Festo SE & Co. KG
BioTech Automation: Learning System
In addition to developing new job profiles, Festo has designed a modular learning concept for the field of biomechatronics. In the learning reactor, this knowledge is taught using a combination of hardware and software