© Festo SE & Co. KG
2023/12/05
|
Globálně
Eichenberger convinces compared to products from the Chinese market
Eichenberger successfully held its own against local Chinese manufacturers in the planning of the new Festo ...
Přečíst tiskovou zprávu
Eichenberger successfully held its own against local Chinese manufacturers in the planning of the new Festo gripper due to outstanding quality (5000% more operational performance in the endurance test), production from a single source, years of expertise and close cooperation throughout the development process from start to finish.   
© Festo SE & Co. KG
Gripper HEPP
Gripper HEPP with spindle from Eichenberger
© Festo SE & Co. KG
2023/11/08
|
Globálně, Německo
A mass flow controller that is silent, fast and cost-effective
 For the gas supply of bioreactors and fermenters or for dosing protective gases - the VEMD mass flow ...
Přečíst tiskovou zprávu
 For the gas supply of bioreactors and fermenters or for dosing protective gases - the VEMD mass flow controller from Festo delivers maximum control dynamics and costs significantly less than comparable solutions for the control of air, oxygen and inert gases.
© Festo SE & Co. KG
VEMD proportional flow control valve
The proportional flow control valve VEMD is a mass flow controller that is silent, dynamic and affordable, and thus ideal for use in the life sciences, food production or biotechnology.
© Festo SE & Co. KG
EHMD in laboratory automation
The compact rotary gripper module EHMD from Festo can handle virtually any gripping task in laboratory automation, no matter how small.  
© Festo SE & Co. KG
2024/05/02
|
Globálně
Reliably gripping and turning small parts
The extremely compact rotary gripper module EHMD is the ideal choice in many life science applications where ...
Přečíst tiskovou zprávu
The extremely compact rotary gripper module EHMD is the ideal choice in many life science applications where small objects need to be gripped and turned in confined spaces. For example, it can be used in laboratory automation to open a variety of sample vials with ease. The Z module automatically adjusts to the thread pitches of the caps, eliminating changeover times.
© Festo SE & Co. KG
Rotary gripper module EHMD
The compact rotary gripper module EHMD comes in a fully electric version or with a pneumatic gripper.
© Festo SE & Co. KG
2024/05/06
|
Globálně
Compact and leak-tight powerhouse
Dosing, aspirating and controlling extremely small quantities of aggressive liquids and gases is not a problem ...
Přečíst tiskovou zprávu
Dosing, aspirating and controlling extremely small quantities of aggressive liquids and gases is not a problem with the media-separated solenoid valve VYKA from Festo. This compact powerhouse has a width of only 7 mm and can dose and aspirate the extremely small amounts of liquid very precisely. It also meets the strict requirements for leak-tightness for gas applications.
© Festo SE & Co. KG
VYKA media-separated solenoid valve
The media-separated solenoid valve VYKA allows the precise dispensing of fluids and the control of liquid flows in manifold duct plates as well as gas flows.