Festo Brings Automated Sample and Liquid Handling Solutions to AACC 2023
Festo features at AACC 2023 Cartesian gantry systems for handling samples and a flexible, high accuracy liquid dispensing system, that enables manufacturers to reduce engineering and procurement overhead while speeding time to market. (Festo AACC [American Association for Clinical Chemistry] Booth #4457, July 23-27, Anaheim Convention Center, Anaheim, Calif.)
The EXCM desktop gantry robot
With the free online productivity tool, Festo Handling Guide Online, manufacturers specify the compact Festo Cartesian gantry system, EXCM, in as little as 20 minutes. At the end of the design session, engineers can download 2 and 3D CAD files of the unit, learn the ship date, and receive a quote. With the CAD files in hand, machine design proceeds while the EXCM ready-to-assemble kit is being prepared for shipment. The EXCM is compact, precise, durable, high speed, quiet, and proven reliable. An EXCM will be dynamically demonstrated at the Festo booth.
Isolation valve for liquid dispensing
VYKA is the company’s precision isolation valve family. With a low impedance coil and configurable hit/hold electronics delivering low heat and high repeatability, VYKA valves are ideal for dispense applications. Dispensed volumes can range from under 1 ul to over 10 ml and up, with an overall coefficient of variation (Cv) under 2% in most cases. VYKA valves are also compact, which means higher density dispensing systems with short fluid paths. VYKA facilitates fast cleaning between various solutions.
The PGVA innovative pressure/vacuum generator
The award-winning Festo PGVA on-board pressure/vacuum generator quietly and energy efficiently generates regulated, filtered air for pressure and vacuum-controlled liquid aspirating and dispensing systems. Within a compact 8"x3"x8" footprint, PGVA comprises an integrated compressor, proportional pressure/vacuum control, air filter, silencer, pressure/vacuum reservoirs, pressure sensor, switching valves, 24V power supply, and digital outlet for valve actuation. PGVA can be controlled from any RS232, USB, or Ethernet port.
For more information on Festo Life Science solutions – dispensing liquids, controlling gases, and handling and gripping vials ‒ email life.sciences.nam@festo.com and visit Festo Laboratory Automation. Visit www.festo.us for the full range of products.
Festo is a leading manufacturer of pneumatic and electromechanical systems, components, and controls for process and industrial automation. For 100 years with more than 50 in the U.S., Festo Corporation has continuously elevated the state of manufacturing with innovations and optimized motion control solutions that deliver higher performing, more profitable automated manufacturing and processing equipment. Through advanced technical and industrial education, Festo Didactic Learning Systems and its partners prepare workers for current and future manufacturing technologies.