© Festo SE & Co. KG
BionicSoftArm 1
The pneumatic lightweight robot BionicSoftArm is flexible from the start and is suitable for direct human-robot collaboration.  
BionicSoftHand
© Festo SE & Co. KG
BionicSoftHand mit neuronalem Netz
BionicSoftHand
BionicSoftHand
© Festo SE & Co. KG
BionicSoftHand
Man and robot hand in hand - the BionicSoftHand allows safe and direct human-machine collaboration.
BionicSoftHand
© Festo SE & Co. KG
BionicSoftHand mit KI
The BionicSoftHand uses artificial intelligence to rotate a multi-sided object so that the blue side is at the top.
BionicSoftArm
© Festo SE & Co. KG
BionicSoftArm Messeexponat
Using the DHEF adaptive gripper, the BionicSoftArm transports several objects at once from one location to another.
© Festo SE & Co. KG
Guinness_World_Records
Der BionicOpter ist seit dem 5. September 2019 im Guinness-Buch der Rekorde zu bestaunen.
BionicOpter
© Festo SE & Co. KG
BionicOpter_1
The highly integrated system of the BionicOpter can be operated easily and intuitively via smartphone.
BionicSoftArm
© Festo SE & Co. KG
BionicSoftArm mit DHAS
The BionicSoftArm with the adaptive gripper DHAS in the human-robot collaboration.
BionicSoftArm
© Festo SE & Co. KG
BionicSoftArm: Teachen über ein Tablet
A motion sequence for the BionicSoftArm can be very easily defined on the tablet.