DPDM Multimount: Festo’s smallest, lightest and easiest-mounting compact cylinder
The new DPDM Multimount compact cylinder is Festo’s smallest, lightest and most economical choice yet in its class.
The new DPDM Multimount compact cylinder is Festo’s smallest, lightest and most economical choice yet in its class. It’s ideal for many applications compact cylinders perform, such as stopping or stabilizing small work pieces or work platforms in light manufacturing. It’s noticeably smaller than Festo’s widely used DMM compact cylinder and unique for the variety of ways it can be fastened in place directly. It can be mounted at the front or rear, vertically or horizontally, hence the “Multimount” in its name. Additionally, all mounting interfaces of the DPDM are compatible with those of the DMM, so it can be considered as a replacement for the latter in some applications. 
The DPDM is available in single- and double-acting versions, with or without protection against rotation, in a variety of common diameters and stroke lengths. There is a variant with heat protection up to 120ºC, and a magnetic piston option for position sensing. The DPDM also can be ordered with a through piston rod for connections at both end of the cylinder, or with a hollow piston rod, which can be used to carry vacuum or compressed air.
Festo at a glance
Festo, the world’s leading supplier of automation technology and technical education, is deploying its products and services to meet the challenges of digitization and smart production. Founded in 1925, the family-owned company based in Esslingen, Germany supports a wide range of needs for advanced solutions in factory and process automation. Festo Canada, celebrating is 50th anniversary this year, has been continuously elevating the state of manufacturing in this country with innovative products, optimized motion control solutions and unrivalled support. Globally, some 300,000 customers put their trust in the company’s pneumatic and electric drive products and technology. In addition, Festo Didactic provides state-of-the-art training equipment and educational programs for industrial companies and educational institutions – about 56,000 customers worldwide. The Festo Group registered sales of €3.45 billion in 2024 financial year and is represented worldwide at 250 locations with about 20,600 employees. More than 8% of its annual turnover is invested in research and development.