This content was translated automatically.

Image
Edelstahl Kombination EPRF EMMH
Owner
Festo SE & Co. KG
ID: 5224

Complete electric solution in hygienic design from a single source

Festo combines the EPRF electric cylinder and the EMMH servomotor, both made of stainless steel
By combining the EPRF electric cylinder and the EMMH servomotor, both made of stainless steel, Festo now offers a high-performance electric drive solution for the food, packaging, and pharmaceutical industries. Together with the appropriate motor cable, the motor, cable, and drive form a fully coordinated, complete hygienic design solution from a single source.

The solution’s particular strength lies in its overall concept: Together with the appropriate motor cable, the EMMH and EPRF form a complete solution consisting of a motor, cable, and drive in a hygienic design, all developed by a single supplier. Users thus benefit from optimally coordinated components, seamless system integration, and high operational reliability. With the new hygienic design solution, Festo supports machine builders and plant operators in designing production processes that are efficient, reliable, and hygienic.

Wherever high standards of hygiene, cleanability, and corrosion resistance are essential, the stainless-steel combination of the EPRF electric cylinder and the EMMH servo motor is exactly the right solution. Both components were developed specifically for hygiene-critical production environments and, with their 316L-grade stainless steel housings and IP69K protection rating, meet the requirements of demanding cleaning processes in food applications and other harsh environments.

High speed and wide temperature range

With a speed of 1 m/s, the electric cylinder is among the fastest on the market. Extremely low and high temperatures ranging from -10 °C to +60 °C have no effect on the drive. The EPRF electric cylinder stands out for its sleek, easy-to-clean design, high corrosion resistance, and flexible integration options. When combined with the EMMH stainless steel servomotor, it creates a high-performance drive system that combines precision, dynamics, and reliability. The perfectly matched components enable easy installation and reduce engineering effort.

EPRF Electric Cylinder | Festo DE

EMMH-AS Servomotor | Festo DE

About Festo

Festo is a global player and an independent family-owned company with headquarters in Esslingen am Neckar, Germany. Festo has set standards in industrial automation technology and technical education ever since its establishment, thereby making a contribution to sustainable development of the environment, the economy and society. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 35 industries. Digitalization, AI and the LifeTech sector with medical technology and laboratory automation are becoming increasingly important. The products and services are available in 176 countries. With about 20,600 employees in over 250 branch offices in around 60 countries worldwide, Festo achieved a turnover of around €3.33 billion in 2025. More than 8% of this turnover is invested in research and development. In this learning company, 1.5 % of turnover is invested in basic and further training. Festo Didactic SE is a leading provider of technical education and training and offers its customers worldwide comprehensive digital and physical learning solutions in the industrial environment.

EPRF electric cylinder and EMMH servomotor
EPRF electric cylinder and EMMH servomotor: a complete electrical solution in a hygienic design from a single source