At SEMICON Europe 2026, Festo will demonstrate how wafers can be moved efficiently, precisely, and reliably through the semiconductor manufacturing process. A networked demonstration system illustrates the complete workflow—from the FOUP through wafer alignment to further processing in wet chemical or vacuum-based applications. Read press release Image Festo SE & Co. KG 11/06/2026 | Global End-to-End Wafer Handling Processes for Greater ... At SEMICON Europe 2026, Festo will demonstrate how wafers can be moved efficiently, precisely, and ... Read press release
By combining the EPRF electric cylinder and the EMMH servomotor, both made of stainless steel, Festo now offers a high-performance electric drive solution for the food, packaging, and pharmaceutical industries. Together with the appropriate motor cable, the motor, cable, and drive form a fully coordinated, complete hygienic design solution from a single source. Read press release Image Festo SE & Co. KG 10/19/2026 | Global Complete electric solution in hygienic design from ... By combining the EPRF electric cylinder and the EMMH servomotor, both made of stainless steel, Festo ... Read press release
The number of vehicles with electric drives worldwide is forecast to grow by around 30% per year until 2030. At the same time, the production processes for the electrified powertrain are changing. While semi-automated production processes have dominated traditional automotive manufacturing with combustion engines up to now, the manufacture of battery cells and electric motors is increasingly developing into fully automated production processes. As a leading manufacturer of automation technology, Festo has the right solutions for this along the... Read press release Image Festo SE & Co. KG 05/29/2026 | Global Everything under control from battery cells to ... The number of vehicles with electric drives worldwide is forecast to grow by around 30% per year ... Read press release
With the blister packaging machine from IWK, sustainability is not just lip service: with recyclable packaging material, low energy consumption, high speed and ergonomics, the CABLIblue 870 card-to-card blister system is proving to be a real trendsetter. The use of electrical automation technology from Festo increases sustainability and efficiency immensely in this application. Read press release Image Festo SE & Co. KG 04/24/2026 | Global How packaging machines are becoming more ... With the blister packaging machine from IWK, sustainability is not just lip service: with recyclable ... Read press release
11/06/2026 | Global Semicon Europe 2026 Semicon Europe is the largest European electronics platform, bringing together industry leaders from across the entire ... Press Releases (2) Images (4) View press kit Image Festo SE & Co. KG
05/29/2026 | Global The Battery Show Europe 2026 Visit Festo at the Stuttgart trade fair in hall 3 at stand E10 Press Releases (4) Images (16) View press kit Image Festo SE & Co. KG
04/24/2026 | Global Interpack 2026 7. until May 13, 2026, Messe Düsseldorf Press Releases (7) Images (16) View press kit Image Festo SE & Co. KG
03/23/2026 | Global LogiMAT 2026 24. - March 26, 2026, Messe Stuttgart. You are cordially invited to visit the Festo stand: Hall 3, Stand 3D29. Press Releases (3) Images (5) View press kit Image Festo SE & Co. KG