ELGD Toothed Belt
© Festo SE & Co. KG
ELGD Toothed Belt
The ELGD electric axis family: ELGD-BS stands for the spindle axes, ELGD-TB for the toothed belt versions
ELGD Toothed Belt
© Festo SE & Co. KG
2024/11/07
|
Global
Precise and dynamic
Innovative guide technology, high rigidity and guide load capacity for more load in the same installation space ...
Read press release
Innovative guide technology, high rigidity and guide load capacity for more load in the same installation space - these are the features of the new ELGD axis family from Festo. In addition, powerful drive elements offer high feed forces and accelerations for shorter cycle times, a long service life and less downtime. A stainless steel cover strip is friction-free on the outside and does not allow any particles to form there. This makes the drives in ...
© Festo SE & Co. KG
2024/09/12
|
Global
Precise control of inert gases
Wherever inert gases need to be precisely controlled, the mass flow controller VEFC from Festo is the right ...
Read press release
Wherever inert gases need to be precisely controlled, the mass flow controller VEFC from Festo is the right choice. Thanks to piezo technology, it is compact and flexible, and offers an excellent price/performance ratio. It is especially suitable for use in electronics manufacturing, food production, and anywhere in machine building where shielding gas is required.
© Festo SE & Co. KG
VEFC mass flow controller
Compact and flexible thanks to piezo technology: the mass flow controller VEFC.
© Festo SE & Co. KG
2024/09/04
|
Ireland, United Kingdom
Festo Controlled Pneumatics
Controlled Pneumatics is the rapidly evolving compressed air technology from Festo that is opening new ...
Read press release
Controlled Pneumatics is the rapidly evolving compressed air technology from Festo that is opening new applications for pneumatics. The technology delivers more precision and control than ever, while having the potential to dramatically reduce energy use. This is clearly demonstrated in the VTEP: the first proportional valve terminal on the market, offering high precision, fast response times, and dynamic control.
© Festo SE & Co. KG
2024/06/06
|
Global
Festo Expands its Portfolio with Multilayer Manifolds
Festo is expanding its portfolio to include multilayer manifolds made of plastic (bonded manifolds) in order to ...
Read press release
Festo is expanding its portfolio to include multilayer manifolds made of plastic (bonded manifolds) in order to be able to offer manufacturers of medical and laboratory equipment solutions from a single source. To this end, Festo is taking over the production systems and processes for manufacturing these complex plastic manifolds from Carville, a leading company in this field.
© Festo SE & Co. KG
Multilayer Manifold
Multilayer manifolds for manufacturers of medical and laboratory equipment: in future, Festo will offer these in combination with media-separated valves from a single source. 
© Festo SE & Co. KG
Battery Recycling
Recovering valuable lithium, cobalt, manganese and nickel from used batteries and reuse them for the production of new batteries: Automated recycling processes enable these rare minerals to be reused economically and cleanly. Festo has the right...
English, British translation unavailable for Jetzt noch mehr hochwertige elektrische Automatisierungstechnik.