© Festo SE & Co. KG
Syntegon - EHPS electric standard gripper from Festo
The electric parallel gripper EHPS from Festo also contributes to the flexibility of the Elematic 3001 WAH case packer by reliably adapting the gripping force to sensitive workpieces.
© Festo SE & Co. KG
2023/05/03
|
Global
Standardisation benefits all packaging lines
Standardisation is a recipe for success for a fruitful collaboration between packaging machine manufacturers ...
Read press release
Standardisation is a recipe for success for a fruitful collaboration between packaging machine manufacturers and automation specialists. The strategic partnership between Syntegon and Festo is a great example of this. Thanks to this cooperation, Syntegon was able to simplify its processes and manage the challenges posed by the pandemic and the supply chain crisis more effectively.
© Festo SE & Co. KG
Syntegon - Valve terminal MPA
The valve terminal MPA from Festo with integrated proportional valves used as standard in the Sepion Coater 175 performs crucial functions. Among other things, it ensures the correct shape of the spray jet and optimum atomisation of the spray...
© Festo SE & Co. KG
Festo Servo Press Kit at Syntegon
Syntegon's RMA uses the modular servo press system YJKP, which is also part of the Festo automation platform. The modular servo press system is a pre-configured modular system consisting of software, controller and standard electric drives.
© Festo SE & Co. KG
Syntegon - RMA (Range Manual Assembly) pilot system
Syntegon's RMA (Range Manual Assembly) pilot system is a highly flexible assembly station for auto-injectors, pens, needle protection systems and other medical devices.
© Syntegon
Syntegon - Sepion Coater
The Sepion Coater series with drum sizes from 175 to 1000 litres is used for coating tablets with films and sugar.
© Festo SE & Co. KG
2023/04/24
|
Global
Extremely high sample throughput rates
If there’s one thing the corona pandemic has taught us, it is that laboratories place tremendous ...
Read press release
If there’s one thing the corona pandemic has taught us, it is that laboratories place tremendous importance on high sample throughput rates. Even with highly qualified laboratory personnel, this demand can no longer be met. There’s no getting round the automation of laboratory processes. That’s why MolGen in the Netherlands developed PurePrep TTR, which can prepare 320 patient samples per hour for molecular downstream processing. And ...
© Festo SE & Co. KG
DHOE pipetting head
An open pipetting system with pipetting head DHOE for simple liquid transport makes it possible to configure the most important pipetting functions based on requirements, and to expand them flexibly – the system is also compatible with the largest...