![](https://pressstorageadmin.blob.core.windows.net/prod/styles/content_header/storage-api-public/field/web_images/VTEM3232Application32Flow32Control.jpg?sv=2017-11-09&sr=b&se=2025-07-21T09:55:09Z&sp=r&sig=q2wG5PgeonaK2P13vf8xlrQyE0TEGuwxu94MTSY69KM%3D&itok=ifMfiTvS)
Control several flow rates simultaneously
The Festo Motion Terminal VTEM combines digitalisation and pneumatics. Quickly activated Motion Apps are revolutionising pneumatics by increasing flexibility and energy efficiency, and accelerating production processes. Thanks to the new Motion App “Flow control”, the VTEM now makes filling containers such as bottles with nitrogen or other gases more profitable and economical.
Digitised pneumatics marks the start of a new age of automation technology. Motion Apps control one piezo valve for almost all pneumatic tasks. Only one piece of hardware is needed for this: the Festo Motion Terminal. The different functions are controlled using Motion Apps. Festo is gradually developing new Motion Apps that are making the Festo Motion Terminal more and more flexible. This reduces complexity and time to market. Digitised pneumatics intelligently connects the mechanical system, electronics and software, and ensures better overall equipment effectiveness (OEE) with lower energy consumption.
Digitised flow control
An application example: nowadays containers for products are often rinsed and filled with gases like nitrogen. With the Motion App “Flow control”, users control the flow rate of compressed air and gases at up to 600 l/min digitally – simultaneously on up to eight independent channels. For precise dosing, the integrated sensors can simply be combined with external flow sensors. This saves energy and costly gases.
Controlling the flow in litres per minute using the app allows the gas to be precisely dosed. The more precisely the filling quantity is defined, the more accurate the filling will be since the percentage deviation from the target quantity can be optimally detected. This flexible, digitised nitrogen control is tamper-proof.
In addition, the app “Selectable pressure level” moves the filling nozzles to the bottles quickly and accurately, and the flexible parameterisation shortens the cycle times. After filling, the filling nozzles are retracted with reduced pressure to save energy.
Software instead of hardware
Thanks to the fast activation of new functions via Motion Apps, machine developers can create a basic machine type using the Festo Motion Terminal and then select the relevant Motion Apps to equip it with different functions and features as per the customer requirements. The ability to copy and transfer parameter sets makes planning easier and saves time. Assigning functions via software has the added benefit of preventing tampering and protecting know-how, since it’s not possible to tell from the outside which functions the valves are executing.
By additionally using the Motion App “Leakage diagnostics” in the application, maintenance is simplified as it automatically monitors for leaks. Malfunctions can thus be detected and pinpointed to a specific actuator using diagnostic cycles and defined threshold values – the reliable basis for predictive maintenance.
Festo is a global player and an independent family-owned company with headquarters in Esslingen am Neckar, Germany. Festo has set standards in industrial automation technology and technical education ever since its establishment, thereby making a contribution to sustainable development of the environment, the economy and society. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 35 industries. Digitalization, AI and the LifeTech sector with medical technology and laboratory automation are becoming increasingly important. The products and services are available in 176 countries. With about 20,600 employees in over 250 branch offices in around 60 countries worldwide, Festo achieved a turnover of around €3.65 billion in 2023. Each year around 7% of this turnover is invested in research and development. In this learning company, 1.5 % of turnover is invested in basic and further training. Festo Didactic SE is a leading provider of technical education and training and offers its customers worldwide comprehensive digital and physical learning solutions in the industrial environment.