2020/07/23
ID: 3259

Festo Motion Terminal and AI driven Dashboards

Herald great strides in process automation

Digitalisation and artificial intelligence (AI) are mega trends that are opening up potential savings in process automation at every phase of a plant's lifecycle. Industrial automation specialist Festo already offers a digital field device, the VTEM Motion Terminal, and Festo Dashboards are available that visualise plant conditions, indicating that AI is becoming a reality in process automation.

Just as the smartphone provides different functions on a standardised hardware platform using apps, Festo’s VTEM Motion Terminal uses the concept of separating hardware and user software. So-called Motion Apps make it possible to carry out 50 different pneumatic applications using just this motion terminal, effectively eliminating the contradiction between standardisation in hardware and flexibility through software.

 

The VTEM Motion Terminal combines mechanical system, electronics and software. Valve terminal technology combined with piezo technology are at the heart of the device, which is equipped with additional sensors. Apps are then used to eliminate the need for additional components, such as traditional limit switch boxes for end position detection for on/off process valves.

 

Save with Apps

Significant savings are possible using this approach. For example, almost every design engineer includes a generous safety reserve when sizing the pneumatic actuators for a plant. As a result, most actuators have more torque and force than required for the actual working movement. This is particularly noticeable in the compressed air consumption of plants in continuous operation. The "ECO drive" Motion App pares down the compressed air consumption caused by the safety factor and the actuator size by reducing the pressure in the actuator to the minimum required for the application movement. Experience has shown that energy savings of up to 50% are possible.

 

Meanwhile, the “Leakage diagnostics” Motion App enables leaks to be detected without interrupting production – saving time and money. Leaks in the compressed air system can be detected and localised to specific actuators through diagnostic cycles. Predefined, precise threshold values thus allow  preventive maintenance and mean that laborious troubleshooting in extended compressed air networks is no longer necessary. Maintenance staff can start working on eliminating the leaks whenever there is a planned break in production.

 

Cloud aids visibility

Festo Dashboards and the CPX-IOT internet gateway are also enabling production managers and operators to detect irregularities at an early stage and initiate the necessary measures before a system failure can occur. These turnkey, preconfigured dashboards do not need any additional programming or installation of software.

 

Further processing and long-term analysis of data can take place on Edge or in the cloud. The data can be called up at any time and visualised via the Festo Dashboard. Plant builders, end users and plant operators can use the comprehensive diagnostics available at any stage to improve condition monitoring and maintenance, or look for energy saving potential – even to compare the process control systems of plants across several locations. The result is increased productivity, greater energy efficiency, less unplanned downtime and major cost savings.

 

AI coming soon

Having the positioner function in a decentralised control unit – in other words not directly at or in the actuator – opens up new horizons, including the use of artificial intelligence. This starts with the decentralised automation of modular plants. When using the International Standards  of ZVEI/NAMUR in their Module Type Package (MTP) approach, a module in higher-level control systems can be easily visualised, and communication can be established at little extra cost.

 

The next step is the decentralised implementation of machine learning algorithms on Edge: in other words at the specific production stage to be monitored. Decentralised monitoring of actuator characteristics, such as pressure in the actuator chambers, travel speeds and their correlation over time, not only enables the parameters of the actuator itself to be analysed, but also allows anomalies in the technical process to be detected. This is the basis for predictive maintenance concepts and for data analyses aimed at optimising the production process. The artificial intelligence in the module controller detects any anomalies without the need for additional programming.

 

The algorithms are taught in based on a database representing normal production, allowing them to independently detect deviations in the production process or in the performance of the actuators. This enables plant operators to detect problems in good time and avoid unscheduled plant downtimes caused by malfunctions.

 

Ends

About Festo 
Festo is a leading international supplier of automation technology with a turnover in 2023 of around €3.65 billion. Festo employs over 20,600 people worldwide and is a proven innovator and problem solver in pneumatic and electrical automation, where it is the performance leader. Festo offers around 33,000 pneumatic and electric products in hundreds of thousands of variants for factory and process automation technology, many of which can be tailored to specific customer needs.  Sustainability, reducing its CO2  footprint, digital learning, innovation, performance and speed are the key drivers for the company's future. Festo GB operates as a carbon neutral organisation and uses the PAS 2060 standard externally audited by NQA to validate this claim to customers, employees and other stakeholders.

Festo Industrial Automation's innovative strength is demonstrated through the launch of around 100 new products every year. The company invests over 7% of its turnover in R&D, resulting in over 2,600 patents held worldwide. For more information about the company's products and UK / Irish services, please visit: www.festo.com/gb  and www.festo.com/ie

Festo and Industry 4.0 - Festo has engaged with the Industry 4.0 initiative from its inception: as a user, manufacturer and trainer.  As a member of the steering group, the company has taken an active role in defining the core standards such as the RAMI model and the Administration Shell.  Festo Didactic has installed Industry 4.0 Cyber-Physical Factory training hardware systems in many leading universities and training centres. It also provides Industry 4.0 training courses for change managers and practical workshops for employees. Industry 4.0 technologies such as OPC-UA communications are embedded in the latest generation products. For more information, go to www.festo.com/digitalisation
 
Festo Didactic training delivers training for industry – by industry. Combining Festo's industrial heritage with its future-focused manufacturing and engineering expertise to deliver courses for greater productivity and competitiveness. Offering a wide range of open courses, structured development programmes and tailor-made, customer-specific projects on technology and Industry 4.0 and the industry-leading online training suite, Festo LX. Festo also provides state-of-the-art training equipment solutions for industrial companies and educational institutions around the world. Festo Didactic has around 56,000 education customers worldwide. More information on Festo training and consulting services can be found at: www.festo.com/didactic

Festo Bionic Learning Network encapsulates the innovative nature of Festo, raising awareness and attracting talent to the company. Exploring the links between nature and technology opens new areas of innovation and demonstrates complex ideas in a stimulating and enjoyable way. Festo works with an alliance of internal R&D, external educational establishments and specialist companies to advance bionic solutions for automation applications of the future. The objective is to benefit from bionics as a source of inspiration and to realise these in industrial automation. For more information about Festo's Bionic Learning Network, please visit: www.festo.com/bionics

 

© Festo SE & Co. KG
Tableros de mandos en la automatización de procesos
Detectar irregularidades en una etapa temprana e iniciar las medidas necesarias antes de que se produzca un fallo en el sistema se puede hacer ahora con los tableros de mandos de Festo.
© Festo SE & Co. KG
Actuadores con unidad de control descentralizada
El hecho de que el posicionador funcione en una unidad de control descentralizada, es decir, no directamente en el actuador, abre nuevos horizontes hasta el uso de la inteligencia artificial.

Persona de contacto global

Descargas

Compartir informe de prensa