© Festo SE & Co. KG
2022/09/20
|
Global
Measuring and weighing without contact
Highly pure, sterile processes are a key challenge for the industrial production – especially in ...
Leer nota de prensa
Highly pure, sterile processes are a key challenge for the industrial production – especially in food processing and the pharmaceuticals and medical technology industries, but also in the electronics sector. To keep manufacturing processes as free from contamination as possible, the workpieces and the workroom should be separated from each other. This can be achieved with superconductor-based levitation. Festo will be showing its concept for ...
© Festo SE & Co. KG
2018/04/02
|
Global
Bionics4Education: Generating enthusiasm for MINT
At the Hannover Messe trade fair, Festo is for the first time presenting a bionic didactic concept that unites ...
Leer nota de prensa
At the Hannover Messe trade fair, Festo is for the first time presenting a bionic didactic concept that unites digital and analogue learning. The objective is to generate enthusiasm among children and adolescents for the natural sciences and technology (MINT). This concept appropriately interlinks bionics and technical education – in the form of a kit for experimenting and learning.
© Festo SE & Co. KG
2022/03/16
|
Global
Interfaces flexibles en la construcción de instalaciones
Flexible, robusta y potente - la válvula de asiento inclinado VZXA de Festo controla los flujos de ...
Leer nota de prensa
Flexible, robusta y potente - la válvula de asiento inclinado VZXA de Festo controla los flujos de medios de forma rápida y fiable hasta a una temperatura de 230 °C. Su arquitectura de producto inteligente con interfaz patentada permite combinar libremente cuerpos de válvulas y actuadores. Con función Hot Swap para la sustitución rápida del actuador o de otras piezas de repuesto.