© Festo SE & Co. KG
Handling Guide Online Screen 1 EN
Handling Guide Online from Festo: allows design and project engineers to configure and order new system solutions intelligently and intuitively – in just 20 minutes.
© Festo SE & Co. KG
Actuadores con unidad de control descentralizada
El hecho de que el posicionador funcione en una unidad de control descentralizada, es decir, no directamente en el actuador, abre nuevos horizontes hasta el uso de la inteligencia artificial.
© Festo SE & Co. KG
VTUG
Quickly connected to all commonly available fieldbuses: the valve terminal VTUG plug-in, as a new family member of the VG series, is electrically modular and pneumatically flexible - also in the control cabinet.
© Festo SE & Co. KG
Electronics manufacturing testing
Electronics manufacturing at the Scharnhausen Technology Plant: Different testing methods ensure high quality. These range from automatic optical inspection (AOI) through in-circuit tests (ICT) to system tests (EOL test).
© Festo SE & Co. KG
Electronics manufacturing SMD devices
Electronics manufacturing at the Scharnhausen Technology Plant: Tens of thousands of units of the CPX are assembled according to customer requirements every year. This requires up to 300 different components, including electronic components such...
© Festo SE & Co. KG
Delta robotics without control cabinet 3
Industry 4.0: the development project can be integrated into a plant as a virtual model.
© Festo SE & Co. KG
Delta robotics without control cabinet 2
Industry 4.0: the development project can be integrated into a plant as a virtual model.
© Festo SE & Co. KG
EMCA 2
Integrated drive EMCA: The brushless DC motors from Festo with absolute position recording, integrated regulator, power electronics, absolute encoders.
© Festo SE & Co. KG
EMCA 1
Integrated drive EMCA: The brushless DC motors from Festo with absolute position recording, integrated regulator, power electronics, absolute encoders.
© Festo SE & Co. KG
CPX automation platform
Integrates the entire electropneumatic control chain: the CPX automation platform.