© Festo SE & Co. KG
Baumer - Marco Ahler
Marco Ahler, director técnico de Baumer hhs
© Festo SE & Co. KG
Baumer - regulador de presión proporcional VPPM
Regulador de presión proporcional VPPM de Festo: la bomba de émbolo DPP regula, en lugar de la presión de líquido, la presión de entrada de aire, con lo que ajusta la presión de líquido deseada. Para ello, el VPPM controla el caudal de aire del...
© Festo SE & Co. KG
Baumer - bomba de doble émbolo DPP
La bomba de doble émbolo DPP de Baumer hhs: es la pieza clave del proceso de encolado – en la parte inferior de la imagen, la válvula proporcional VPPM de Festo.
© Festo SE & Co. KG
Baumer - encolado de alta precisión
Encolado de cajas plegables de alta precisión: los sistemas de Baumer hhs ofrecen un encolado milimétrico sin contacto con el recorte incluso a la máxima velocidad de producción.
Frugalpac 5
Festo’s CPX-E-CEC Controller regulates multiple axes simultaneously to achieve the complex curves on the glue paths, while Festo CMMT servo controllers are used for precise and repeatable loading, gluing and unloading.
Frugalpac 4
Frugal Bottles are manufactured from two paperboard blanks and require complex gluing patterns that can be tailored to different profiles.  
© Festo SE & Co. KG
2022/09/10
|
Global
Remote IO system taken to a whole new level
The decentralised IO system CPX-AP-I allows compact and lightweight I/O modules as well as the decentralised ...
Leer nota de prensa
The decentralised IO system CPX-AP-I allows compact and lightweight I/O modules as well as the decentralised valve terminals from Festo to be integrated into major host systems in a flexible and scalable way. Another advantage of CPX-AP-I is its seamless connectivity from the field level right through to the cloud, providing access to features such as predictive maintenance. This makes digitalisation incredibly easy.
© Festo SE & Co. KG
CPX-AP-I
A remote IO system that is all set for the future of digitalisation: CPX-AP-I from Festo. (Photo: Festo SE & Co. KG)
© Festo SE & Co. KG
2022/09/20
|
Global
From the blank to the bottle under high pressure
Thanks to high-pressure pneumatics, stretch blow moulding machines achieve an output per blow moulding station ...
Leer nota de prensa
Thanks to high-pressure pneumatics, stretch blow moulding machines achieve an output per blow moulding station of between 1,000 and nearly 3,000 PET bottles per hour. The key to this success is precise control using valves and valve blocks and the proper compressed air preparation. These are supplied by Festo, along with global services, from design engineering tools to operation. At drinktec in Munich in September 2022, innovative digitalisation ...
© Festo SE & Co. KG
High pressure valve block
Precise control for high-pressure pneumatics – with a valve block from Festo.