© Adolf Würth GmbH & Co. KG
Festo and Würth innovation partnership_Image 2
The customized Festo GripperAI solution can grip almost anything you put in front of it - and what the gripper and robot are designed for. The grippers specially developed for this project set new standards in robot technology, while the suction...
© Festo SE & Co. KG
VTEP - uso en fotolitografía
Válvulas como la VTEP también se utilizan como válvulas piloto para válvulas de medios. En fotolitografía, por ejemplo, los wafern deben recubrirse con gran precisión con una laca resistente a la luz. Una función de aspiración hacia atrás...
© Festo SE & Co. KG
Pulir wafern con VTEP
Regulación de alta precisión de 5 zonas de presión para un pulido extremadamente suave al pulir wafern con VTEP.
© Festo SE & Co. KG
Terminal de válvulas proporcionales VTEP
Muy compacto: 10 canales de trabajo en un ancho de menos de 120 mm
© Adolf Würth GmbH & Co. KG
Festo and Würth innovation partnership_Image 1
Festo developed an AI robot solution for Würth that efficiently handles heavy parts and various objects in particular, thus significantly reducing the workload on employees and increasing efficiency in operations.
© Adolf Würth GmbH & Co. KG
2024/06/28
|
Global
Festo develops AI robot solution for logistics center at Würth
The innovation partnership between Festo and Würth has already lasted two years, and the first phase of ...
Leer nota de prensa
The innovation partnership between Festo and Würth has already lasted two years, and the first phase of the partnership is now coming to an end – with success: the prototype works. Würth wants to comprehensively test Festo's tailor-made AI software solution at the Reinhold Würth Innovation Center Curio, discuss it with employees and, if everything proves successful, implement it in its logistics centers worldwide.
Español translation unavailable for Dalla piattaforma CPX-AP-A all'unità valvole VTUG.
Español translation unavailable for Produzione sicura di idrogeno mediante elettrolisi.
Español translation unavailable for Idrogeno verde per diversi settori industriali.
Español translation unavailable for Immagazzinare l'idrogeno verde.