© Festo SE & Co. KG 2024/05/06 | Globale, Allemagne A real modular DNA factory Seeds are the new gold. Why is that? Plant-based foods can feed an ever-growing world population. But climate ... Lire le communiqué de presse Seeds are the new gold. Why is that? Plant-based foods can feed an ever-growing world population. But climate change, pests and diseases threaten plant breeding. To help develop resistant seeds and make them available to agriculture, plant breeders need vast amounts of DNA. That is precisely why Synchron Lab has developed the "DNA factory", which is automated with handling gantries, electric axes, pneumatic grippers and sensors from Festo.
© Festo SE & Co. KG 2022/11/11 | Globale Playing it safe in the assembly of MRI machines The future belongs to human-robot cooperation. System builder BEC developed such a collaborative solution for ... Lire le communiqué de presse The future belongs to human-robot cooperation. System builder BEC developed such a collaborative solution for Siemens Healthineers. It inserts coils weighing several tonnes precisely into the magnets of magnetic resonance imaging (MRI) machines. Electric cylinders from Festo, which ensure the coils are securely gripped, play a crucial role here.
© Festo SE & Co. KG 2022/10/19 | Globale Festo’s new ELGT cantilever electro-mechanical drive Industrial automation specialist Festo has introduced a new cantilever electro-mechanical drive that is ... Lire le communiqué de presse Industrial automation specialist Festo has introduced a new cantilever electro-mechanical drive that is designed to meet the demanding specifications of modern production facilities. The new ELGT drive combines precision with high load-bearing capacity and rigidity, which makes it ideal for small parts and Lithium-ion battery manufacturing.
© Festo SE & Co. KG 2021/06/25 | Globale Economique et ouvert à de nombreux fournisseurs Les axes à vis compacts et économiques ELGT de Festo avec double guidage intégré ... Lire le communiqué de presse Les axes à vis compacts et économiques ELGT de Festo avec double guidage intégré sont parfaits pour être combinés dans des systèmes de porte-à-faux 2D et 3D. Développés pour des applications dans l'industrie électronique, dans les applications de bureau et dans la fabrication de batteries, ils sont ouverts aux servomoteurs Festo ainsi qu'à de nombreux autres ...
2024/11/08 | Globale SPS 2024 - The Automation ... The SPS from 12 – 14 November 2024 in Nuremberg is the industry highlight of the automation sector ... Communiqués de presse (7) Illustrations (11) Vidéos (0) Voir le dossier de presse © Festo SE & Co. KG