Precisely gluing smartphone displays, applying thermal paste or gluing micro cameras in place are just a selection of the adhesive processes that represent the dosing and dispensing competencies of ViscoTec. Now the company has brought out cartridge applicator units designed for exact and clean feeding of adhesives, pastes and silicones of different viscosities, supported by a pneumatic control module supplied by Festo right to the ViscoTec assembly line as a ready-to-install module. Lire le communiqué de presse Image Festo SE & Co. KG 2021/11/09 | Global High-precision dosing with different viscosities Precisely gluing smartphone displays, applying thermal paste or gluing micro cameras in place are ... Lire le communiqué de presse
Highly flexible and modular production plants with decentralised automation enable the process industry to react to fluctuations in demand. This is the case in water treatment, in the pharmaceutical, fine chemical and food industries and also in energy generation. Decentralised controllers from Festo are perfect for this. Festo developed the PA-Toolkit for programming these controllers to enable simple application engineering in line with the “Module Type Package” (MTP) from Namur and ZVEI. Lire le communiqué de presse Image Festo SE & Co. KG 2020/07/20 | Globale Simplified integration into control systems Highly flexible and modular production plants with decentralised automation enable the process ... Lire le communiqué de presse
2022/11/03 | Globale SPS 2022 - Smart Production Solutions Nuremberg, Germany from 8 to 10 November 2022 - Festo in Hall 9 Booth 361 Communiqués de presse (3) Images (14) Voir le dossier de presse Image Festo SE & Co. KG