Wind energy
© WorldSkills
Skill 62 Renewable Energy
The Nacelle wind turbine learning system was developed specifically for training wind technicians to provide the growing market of renewable energy with the skilled workers it needs.
Water Technology
© WorldSkills
Skill 55 Water Technology
The water management topic maps the water cycle of a water and wastewater treatment plant.
Industry 4.0
© WorldSkills
Skill 48 Industry 4.0
Industry 4.0 stands for the 4th transformation in the history of factory automation. Its main goal is to optimize networked production and save time and money.
Skill 04 Mechatronics
© WorldSkills
Skill 04 Mechatronics
Mechatronics combines different technologies such as mechanics, electronics, and information technology.
Skills change the world
© WorldSkills
2022/09/22
|
Globale
WorldSkills Competition 2022 Special Edition in Stuttgart
After the cancellation of WorldSkills 2022 in Shanghai due to COVID-19 restrictions in China, new opportunities ...
Lire le communiqué de presse
After the cancellation of WorldSkills 2022 in Shanghai due to COVID-19 restrictions in China, new opportunities came up for the WorldSkills competition: The WorldSkills Competition 2022 Special Edition will be held decentralized in 15 countries. Germany benefits directly from this: 9 of 62 competitions will take place in Germany, three of them in Stuttgart, at the beginning of October parallel to the Motek and Vision industrial trade fairs. This gives ...
© Festo SE & Co. KG
2022/09/10
|
Globale
Remote IO system taken to a whole new level
The decentralised IO system CPX-AP-I allows compact and lightweight I/O modules as well as the decentralised ...
Lire le communiqué de presse
The decentralised IO system CPX-AP-I allows compact and lightweight I/O modules as well as the decentralised valve terminals from Festo to be integrated into major host systems in a flexible and scalable way. Another advantage of CPX-AP-I is its seamless connectivity from the field level right through to the cloud, providing access to features such as predictive maintenance. This makes digitalisation incredibly easy.
© Festo SE & Co. KG
CPX-AP-I
A remote IO system that is all set for the future of digitalisation: CPX-AP-I from Festo. (Photo: Festo SE & Co. KG)
© Festo SE & Co. KG
2022/09/20
|
Globale
From the blank to the bottle under high pressure
Thanks to high-pressure pneumatics, stretch blow moulding machines achieve an output per blow moulding station ...
Lire le communiqué de presse
Thanks to high-pressure pneumatics, stretch blow moulding machines achieve an output per blow moulding station of between 1,000 and nearly 3,000 PET bottles per hour. The key to this success is precise control using valves and valve blocks and the proper compressed air preparation. These are supplied by Festo, along with global services, from design engineering tools to operation. At drinktec in Munich in September 2022, innovative digitalisation ...
© Festo SE & Co. KG
High pressure valve block
Precise control for high-pressure pneumatics – with a valve block from Festo.
© Festo SE & Co. KG
High pressure lab
High-pressure laboratory at Festo: here, components of high-pressure pneumatics up to 40 bar are developed for the production of PET bottles in the stretch blow moulding process for linear and rotary machines.