SupraCube
© Festo SE & Co. KG
2021/04/12
|
Globale
SupraCube: Maximum flexibility in automation technology
With the SupraCube, Festo is presenting for the first time a SupraMotion concept in which the superconductor ...
Lire le communiqué de presse
With the SupraCube, Festo is presenting for the first time a SupraMotion concept in which the superconductor unit can be separated from the electrical cooler and can operate autonomously for up to two hours. The compact technology allows contactless movement and handling of objects - ideal for industries with the highest requirements for cleaning and cleanliness, such as laboratory automation, biotechnology or semiconductor production.
2020/02/27
|
Irlande, Grande-Bretagne
Festo invests to meet growing demand for electronics components
The semiconductor and electronics industries have set benchmarks for continuous innovation while keeping prices ...
Lire le communiqué de presse
The semiconductor and electronics industries have set benchmarks for continuous innovation while keeping prices low. As digitalisation increases, electronic components are rapidly finding their way into other industries too. Sectors as diverse as the automotive industry, medical technology and distribution logistics are demanding more powerful electronics and sensors for applications ranging from self-driving vehicles to artificial heart valves. ...
electronic components Pic 3
"Festo has doubled its production capacity worldwide, which means it is now prepared for the high demand for electric and pneumatic standard products." Arian Scholz, Head of Global Key Account and Industry Segment Management at Festo.
electronic components DGST Pic 2
The DGST mini slide is one of more than 2,200 electronic components in Festo’s core product range that cover every phase of the pneumatic and electrical control chain.
electronic components Pic 1
Festo has invested significantly in its core product range and related manufacturing and supply network to ensure that its electronic components are readily available worldwide.
VEMD: proportional control valve pic 2
Extremely high control dynamics: the VEMD proportional flow control valve is ideal for regulating gas flows in ventilation treatment.
© Festo SE & Co. KG
2020/08/04
|
Globale
Un robot de manipulation sur mesure en seulement 20 minutes
Avec Handling Guide Online (HGO), les constructeurs de machines peuvent concevoir le système de ...
Lire le communiqué de presse
Avec Handling Guide Online (HGO), les constructeurs de machines peuvent concevoir le système de manipulation prêt-à-installer Festo en un temps record. Que ce soit pour un système mono-axe, un portique linéaire, 2D ou tri-dimensionnel. Ils peuvent commander leur solution système de manière intelligente et intuitive directement en ligne, car la plateforme de configuration est ...
© Festo SE & Co. KG
Electronics manufacturing testing
Electronics manufacturing at the Scharnhausen Technology Plant: Different testing methods ensure high quality. These range from automatic optical inspection (AOI) through in-circuit tests (ICT) to system tests (EOL test).
© Festo SE & Co. KG
Electronics manufacturing SMD devices
Electronics manufacturing at the Scharnhausen Technology Plant: Tens of thousands of units of the CPX are assembled according to customer requirements every year. This requires up to 300 different components, including electronic components such...