CMMT-ST
Stepper or Servo? The new CMMT-ST from Festo gives the best of both worlds
© Festo SE & Co. KG
BEC – Servo drive CMMT-ST
Practical: the drive amplifiers, in this case the servo drives CMMT-ST, are mounted on the robot itself, rather than on the gripper system. This frees up space on the gripper and makes it less complicated.
© Festo SE & Co. KG
BEC – Insertion of coils into the magnets
Collaborative solution: coils weighing several tonnes are inserted precisely into the magnets of magnetic resonance imaging machines.
2021/10/20
|
Irlande, Grande-Bretagne
Grolsch bottling plant upgrade goes with a swing, thanks to Festo automation
New servo technology from Festo is helping Grolsch to put the iconic swing tops on its bottles of lager. The ...
Lire le communiqué de presse
New servo technology from Festo is helping Grolsch to put the iconic swing tops on its bottles of lager. The ‘swing-top transfer unit’ was custom-designed by Festo in conjunction with system integrator MCA Linear Motion Robotics and is installed at the Grolsch Enschede plant in The Netherlands.
© Festo SE & Co. KG
Grolsch pic 2
The Grolsch 'swing-top transfer unit' features the new Festo EMMT servo motor and CPX-E automation system and provides approximately 3,800 bottles per hour with a porcelain cap and rubber ring.
Grolsch pic 1
New servo technology from Festo is helping Grolsch to put the iconic swing tops on its bottles of lager.
Servo drives developer kit
The Festo developer kit provides a risk-free application development tool that enables users to familiarise themselves with the functions and application possibilities of the company’s CMMT servo drives.
© Festo SE & Co. KG
2020/01/23
|
Irlande, Grande-Bretagne
Festo introduces a compact servo drive for demanding positioning applications
Festo has expanded its range of servo drives with the introduction of the CMMT-ST. Complementing the existing ...
Lire le communiqué de presse
Festo has expanded its range of servo drives with the introduction of the CMMT-ST. Complementing the existing CMMT-AS, this new servo drive is equally reliable but much more compact and economical.  These characteristics make it ideal for point-to-point and interpolating motion in demanding applications in assembly and handling technology, packaging machines or in the electronics industry.
© Festo SE & Co. KG
CMMT-ST compact servo drive
The CMMT-ST compact servo drive from Festo offers extremely economical positioning and motion.