From consistent data to lifelong added value
From digital twins to efficient circuit diagrams, from design tools to maximum energy savings – Festo supports its customers holistically and in every phase of their value creation process. This extends to the circular economy and the product carbon footprint, but also to lifelong learning with digital training tools for both trainees and long-term employees.
Automation engineers can realize great savings potential right from the start of a machine's design. With appropriate sizing tools, digital twins and efficient circuit diagrams, savings of up to 80% can be achieved by correctly dimensioning the drives, planning downstream AI monitoring of the machine or importing data via digital twins. Design tools such as Electric Motion Sizing for optimal drive and mechanical dimensioning, Handling Guide Online for simple multi-axis cartesian engineering or FluidDraw for electrical and pneumatic circuit diagrams are just a few examples of the many calculation tools that Festo uses to make planning and design easier for its customers.
Savings potential through digitalization and AI in the ongoing production process
The digital maintenance tool Festo AX Smartenance and the Festo AX Industrial Intelligence software enable networked production monitored by AI. This empowers customers to save up to 50% of resources through more efficient processes together with reducing unplanned downtimes by up to 25%.
Festo AX Smartenance is a CMMS (Computerized Maintenance Management System) software and combines maintenance, servicing, spare parts management and machine logbook in one solution. The web application for maintenance or production managers and the mobile app for maintenance staff and machine operators ensures that all relevant information about a machine can be called up anytime and anywhere.
Avoiding unplanned downtimes, ensuring product quality and reducing energy costs – Festo AX Industrial Intelligence makes it all possible. "AI supports our customers in terms of solution design, energy consumption and preventive maintenance. Festo plays a leading role when it comes to AI in the industrial environment. These are skills that are based on years of expertise and inventiveness at Festo," explains Gerhard Borho, Member of the Management Board for IT and Digitalization at Festo.
New are pre-trained AI apps that can even be used by users without extensive AI expertise. This enables companies to record real-time data from production processes and analyze it with the help of AI.
The use of AI enables,
- predictive maintenance to reduce downtimes by up to 25%
- optimized product quality assurance (predictive quality) and thus reduces rejects by up to 20%
- The more efficient use of resources (predictive energy) by reducing leakages by up to 65%.
Integrating sustainability: smarter, greener industrial automation
The product carbon footprint (PCF) describes the effect the CO₂ consumption of the product has on the environment throughout its product lifecycle. A simple example: Festo offers repair kits for many products. Through these repairs 90% CO₂ can be saved throught the product lifecycle compared to buying a replacement part. All the data on Festo's products is available in Festo AX Smartenance. If you combine the circular economy with digitalization, all the data from design and operation can be used via an enriched digital twin.
Lifelong learning: a "must" in the age of digitalization
From tailor-made learning packages and digital platforms to complete training centers, Festo Didactic supports automation customers who want to equip their trainees and employees with new and essential digitalization skills. The experts combine their industry expertise with didactic know-how to ensure employability in high-tech industries. Festo LX, the interactive learning portal, is based on multimedia learning content that can be edited in modules and combined to create individual learning paths.
Tailored learning formats adapt to the learning situation. The so-called eLab courses are mainly used in vocational training in combination with physical learning systems. Pure e-learning courses, on the other hand, can be used without a learning system and accompany learners beyond the field of training and into continuing professional development.
Festo è un attore globale e un'azienda indipendente a conduzione familiare con sede a Esslingen am Neckar, in Germania. Fin dagli inizi Festo ha stabilito degli standard nella tecnologia dell'automazione industriale e nella formazione tecnica, contribuendo così allo sviluppo sostenibile dell'ambiente, dell'economia e della società. Prodotti e servizi sono disponibili in 176 paesi del mondo. L'azienda, infatti, fornisce tecnologia di automazione pneumatica ed elettrica a 300.000 clienti di automazione di fabbrica e di processo in oltre 35 industrie. Il settore LifeTech con la tecnologia medica e l'automazione di laboratorio sta diventando sempre più importante. Con circa 20.600 dipendenti in oltre 250 filiali in circa 60 paesi in tutto il mondo, Festo ha realizzato un fatturato di circa 3,45 miliardi di euro nel 2024. Ogni anno oltre l'8% di questo fatturato viene investito in ricerca e sviluppo, mentre l'1,5 % del fatturato è investito nella formazione di base e di perfezionamento. Festo Didactic SE è un fornitore leader di formazione e formazione tecnica e offre ai suoi clienti in tutto il mondo soluzioni complete di apprendimento digitale e fisico in ambiente industriale.