© Festo SE & Co. KG
Handling Guide Online Screen 1 EN
Handling Guide Online from Festo: allows design and project engineers to configure and order new system solutions intelligently and intuitively – in just 20 minutes.
© Festo SE & Co. KG
2021/05/25
|
ワールドワイド
Great strides into the digital future
Digitalisation and artificial intelligence (AI) are mega trends that are also opening up the potential for ...
プレスリリースを閲覧する
Digitalisation and artificial intelligence (AI) are mega trends that are also opening up the potential for savings in all phases of a plant's lifecycle in process automation. A digital field device, the Festo Motion Terminal VTEM, is already available. Festo Dashboards also visualise plant conditions and even artificial intelligence is no longer far removed from becoming a reality in process automation.
© Festo SE & Co. KG
Actuators with decentralised control units
Having the positioner function in a decentralised control unit, in other words not directly at or in the actuator, opens up new horizons right up to the use of artificial intelligence.
© Festo SE & Co. KG
Dashboards in process automation
Detecting irregularities at an early stage and initiating the necessary measures before a system failure can now be done with the dashboards from Festo.
© Festo SE & Co. KG
VTUG
Quickly connected to all commonly available fieldbuses: the valve terminal VTUG plug-in, as a new family member of the VG series, is electrically modular and pneumatically flexible - also in the control cabinet.
© Festo SE & Co. KG
Electronics manufacturing testing
Electronics manufacturing at the Scharnhausen Technology Plant: Different testing methods ensure high quality. These range from automatic optical inspection (AOI) through in-circuit tests (ICT) to system tests (EOL test).
© Festo SE & Co. KG
Electronics manufacturing SMD devices
Electronics manufacturing at the Scharnhausen Technology Plant: Tens of thousands of units of the CPX are assembled according to customer requirements every year. This requires up to 300 different components, including electronic components such...
© Festo SE & Co. KG
Delta robotics without control cabinet 3
Industry 4.0: the development project can be integrated into a plant as a virtual model.
© Festo SE & Co. KG
Delta robotics without control cabinet 2
Industry 4.0: the development project can be integrated into a plant as a virtual model.
© Festo SE & Co. KG
EMCA 2
Integrated drive EMCA: The brushless DC motors from Festo with absolute position recording, integrated regulator, power electronics, absolute encoders.