© Syntegon
Servo Press Kit YJKP at Syntegon
The servo press kit YJKP performs three joining and pressing steps: from inserting the cartridge, needle and spring to inserting the glass and plastic covers (Photo: Syntegon)  
© Syntegon
Syntegon assembly line for insulin pens
General view of the new machine: Syntegon's automatic assembly lines produce up to 300 insulin pens per minute, depending on the model. The degree of automation is scalable according to requirements and can also be adapted at a...
© Festo SE & Co. KG
2021/03/02
|
ワールドワイド
Highly flexible pick & place with digitised pneumatics
The Festo Motion Terminal VTEM combines digitalisation and pneumatics. Quickly activated Motion Apps are ...
プレスリリースを閲覧する
The Festo Motion Terminal VTEM combines digitalisation and pneumatics. Quickly activated Motion Apps are revolutionising pneumatics by increasing flexibility and energy efficiency, and accelerating production processes. This also has benefits for handling technology, because the automation platform VTEM opens the door for positioning using pneumatics.
© Festo SE & Co. KG
Application Festo Motion Terminal VTEM pick & place
Highly flexible pick & place: the Festo Motion Terminal positions using pneumatics.
Japanese translation unavailable for Festo’s DLGF flat design rodless drive fits tight spaces and budgets.
Japanese translation unavailable for DLGF.
Japanese translation unavailable for Festo Showcases its Latest Automation Innovations at Pack Expo Connects.
© Festo SE & Co. KG
PROFINET bus interfaces from Festo
The new PROFINET bus interfaces from Festo: new features for more applications, including in the process industry.
© Festo SE & Co. KG
Valve terminal CPX-MPA with bus module
Valve terminal CPX-MPA with the new bus module CPX-FB43: Festo has upgraded its PROFINET bus interfaces for the CPX automation platform.