© Syntegon
Syntegon - Sepion Coater
The Sepion Coater series with drum sizes from 175 to 1000 litres is used for coating tablets with films and sugar.
© Festo SE & Co. KG
2024/05/06
|
ワールドワイド
Extremely high sample throughput rates
If there’s one thing the corona pandemic has taught us, it is that laboratories place tremendous ...
プレスリリースを閲覧する
If there’s one thing the corona pandemic has taught us, it is that laboratories place tremendous importance on high sample throughput rates. Even with highly qualified laboratory personnel, this demand can no longer be met. There’s no getting round the automation of laboratory processes. That’s why MolGen in the Netherlands developed PurePrep TTR, which can prepare 320 patient samples per hour for molecular downstream processing. And ...
© Festo SE & Co. KG
DHOE pipetting head
An open pipetting system with pipetting head DHOE for simple liquid transport makes it possible to configure the most important pipetting functions based on requirements, and to expand them flexibly – the system is also compatible with the largest...
© Festo SE & Co. KG
MolGen - Pipetting
Extremely small pipetting volumes: the second robot arm with the pipetting head distributes liquids onto a microwell plate.
© Festo SE & Co. KG
MolGen - Opening vial
During the initial work operation, the first robot arm grasps a sample vial by the cap with an electric gripper and brings it into a position at which the cap is removed.
© Festo SE & Co. KG
MolGen - Gripping vial
During the initial work operation, the first robot arm grasps a sample vial by the cap with an electric gripper and brings it into a position at which the cap is removed.
© Festo SE & Co. KG
MolGen - PurePrep TTR
High throughput: the fully automated PurePrep TTR system prepares 320 patient samples per hour for PCR testing. Laboratory-specific automation technology from Festo is included.
© Festo SE & Co. KG
Dr. Jan Seyler
Dr. Jan Seyler, Head of Advanced Analytics and Control at Festo
© Festo SE & Co. KG
The Festo cobot and GripperAI in logistics
The Festo GripperAI uses its own neural network to calculate gripping points. It can even distinguish between different gripping techniques and change the tools itself.