© Festo SE & Co. KG
Technology Plant Scharnhausen
The Scharnhausen Technology Plant – the Festo production site for valves, valve terminals and electronics.
© Festo SE & Co. KG
Lean and Green Award Presentation 2016
The Scharnhausen Technology Plant has been announced as the winner of the special prize category of the "Lean & Green Management Awards 2016". The official awards presentation took place on 5 and 6 December 2016 at the Blaichach/Immenstadt site of...
© Festo SE & Co. KG
2021/11/15
|
ワールドワイド
The right handling system in a matter of minutes
With the Handling Guide Online, design engineers can create the right ready-to-install handling system from ...
プレスリリースを閲覧する
With the Handling Guide Online, design engineers can create the right ready-to-install handling system from Festo in record time, whether for a 2D linear and planar surface gantry, a 3D gantry or a new 3D cantilever system. Not only can they now plan extremely compact or extremely dynamic Cartesian robots using the intuitive configuration and ordering software, but they also benefit from the circuit diagram service from Eplan and commissioning files.
© Festo SE & Co. KG
Handling Guide Online
With the Handling Guide Online, machine and system builders are able to reduce their time to market for integrated handling systems by up to 70%.
© Festo SE & Co. KG
FinRay Gripper
The FinRay gripper from Festo offers gripper fingers that adapt to the workpiece. This allows safe and tactile gripping of workpieces with plastic malleability such as pouch cells.
© Festo SE & Co. KG
CPX-AP-I
The remote IO system CPX-AP-I seamlessly integrates all IOs and IO-Link participants such as sensors and valve terminals into the communication network of the plant. This ensures seamless communication from the workpiece to the cloud.
© Festo SE & Co. KG
Cantilever handling system spindle axes ELGT
A cantilever handling system based on spindle axes ELGT ensures dynamic and safe loading and unloading of the process chamber.
© Festo SE & Co. KG
Degassing process chambers
The core of the application is the process chamber. Pneumatic and electric actuators manipulate hollow lances and pierce the battery cells.
© Festo SE & Co. KG
2023/05/15
|
ワールドワイド
Reliable degassing in battery cell production
Degassing and sealing are core processes in battery cell production that directly follow the initial contacting ...
プレスリリースを閲覧する
Degassing and sealing are core processes in battery cell production that directly follow the initial contacting of the battery cells with electrical voltage. The battery cells are pierced with lances and the forming gas produced during contacting is extracted. Pneumatic and electric actuators from Festo are used to handle and pierce the battery cells.
Japanese translation unavailable for Automation trifft Online Experience .