© Festo SE & Co. KG
DGTZ twin cylinder
The versatile twin cylinder DGTZ with four mounting surfaces, three payload attachment surfaces and two sensor attachment surfaces.
© Festo SE & Co. KG
2024/01/23
|
ワールドワイド
Reliable gripping without air
The electric standard gripper EHPS from Festo is the electric version of the pneumatic standard gripper DHPS. ...
プレスリリースを閲覧する
The electric standard gripper EHPS from Festo is the electric version of the pneumatic standard gripper DHPS. The EHPS can be used wherever pneumatics is not permissible. The concept of the electric standard gripper is based on simplicity and low complexity – all the electronics are integrated in the gripper, which means that an external motor controller is not required.
© Festo SE & Co. KG
EHPS electric standard gripper
The electric parallel gripper variant EHPS-…-LK with integrated memory for various learning functions.
© Festo SE & Co. KG
DSNU-S round cylinder
The round cylinder DSNU-S-…: the slimmer and shorter version of the standards-based cylinder DSNU.
© Festo SE & Co. KG
CECC controller
IO-Link Master with CECC controller: Competent and consistent decentralisation of an installation can be achieved with the compact controller CECC with four IO-Link master ports.