SupraMultitool
© Festo SE & Co. KG
SupraMultitool
At the SupraMultitool exhibit, a handling system positions a workpiece carrier on two different magnets in turn.
SupraModule
© Festo SE & Co. KG
SupraModule_4
With the SupraModule, different applications can be carried out with the same system in a floating position and controlled wirelessly. Depending on requirements, different systems can be attached to the carrier, for example a compact gripper.
SupraModule
© Festo SE & Co. KG
SupraModule_3
With the SupraModule, different applications can be carried out with the same system in a floating position and controlled wirelessly. Depending on requirements, different systems can be attached to the carrier, for example a compact gripper.
SupraModule
© Festo SE & Co. KG
SupraModule_2
With the SupraModule, different applications can be carried out with the same system in a floating position and controlled wirelessly. Depending on requirements, different systems can be attached to the carrier, for example a compact gripper.
SupraModule
© Festo SE & Co. KG
SupraModule 1
With the SupraModule, different applications can be carried out with the same system in a floating position and controlled wirelessly. Depending on requirements, different systems can be attached to the carrier, for example a compact gripper.
SupraModule
© Festo SE & Co. KG
2023/03/13
|
ワールドワイド
SupraModule: Modulare Lösung für die Laborautomation
In future-oriented fields such as laboratory automation or biotechnology the requirements placed on the ...
プレスリリースを閲覧する
In future-oriented fields such as laboratory automation or biotechnology the requirements placed on the cleaning of production facilities and their purity are very high. With superconductor technology, objects can be moved and handled without contact, which is ideal for such applications. At the Hannover Messe 2020 trade fair, Festo will be presenting the SupraModule concept, which enables wireless control of functions on a magnetic, floating carrier ...
© Festo SE & Co. KG
Handling Guide Online Monitor 1
With the Handling Guide Online, machine and system builders are able to reduce their time to market for integrated handling systems by up to 70%.
© Festo SE & Co. KG
CPX-AP-I
A remote IO system that is all set for the future of digitalisation: CPX-AP-I from Festo.
© Festo SE & Co. KG
Kia wheel fitting
The balancer’s ergonomic benefits also come into their own when fitting wheels in Kia Motors’ car production plant in Slovakia. (Photo: Kia Motors Slovakia)
© Festo SE & Co. KG
Kia door fitting
Kia Motors Slovakia counts on the balancer for fitting doors in its vehicle production. (Photo: Kia Motors Slovakia)