© Festo SE & Co. KG
HAHN Automation Group - 3-axis gantry from Festo
In central stage: a 3-axis gantry for optical and leak tests, consisting of electric drives from Festo.
© Festo SE & Co. KG
HAHN Automation Group - End-of-line test system
All relevant test scenarios for 90% of all battery packs available on the market can be implemented on the end-of-line test system.
© Festo SE & Co. KG
HAHN Automation Group - Battery tester EOLT
Fully automated 100% testing of battery cells: with the EOLT battery tester from HAHN Automation Group  
© Festo SE & Co. KG
Syntegon - EHPS electric standard gripper from Festo
The electric parallel gripper EHPS from Festo also contributes to the flexibility of the Elematic 3001 WAH case packer by reliably adapting the gripping force to sensitive workpieces.
© Festo SE & Co. KG
2024/03/28
|
ワールドワイド
Standardisation benefits all packaging lines
Standardisation is a recipe for success for a fruitful collaboration between packaging machine manufacturers ...
プレスリリースを閲覧する
Standardisation is a recipe for success for a fruitful collaboration between packaging machine manufacturers and automation specialists. The strategic partnership between Syntegon and Festo is a great example of this. Thanks to this cooperation, Syntegon was able to simplify its processes and manage the challenges posed by the pandemic and the supply chain crisis more effectively.
© Festo SE & Co. KG
Festo Servo Press Kit at Syntegon
Syntegon's RMA uses the modular servo press system YJKP, which is also part of the Festo automation platform. The modular servo press system is a pre-configured modular system consisting of software, controller and standard electric drives.
© Festo SE & Co. KG
Syntegon - RMA (Range Manual Assembly) pilot system
Syntegon's RMA (Range Manual Assembly) pilot system is a highly flexible assembly station for auto-injectors, pens, needle protection systems and other medical devices.
© Syntegon
Syntegon - Sepion Coater
The Sepion Coater series with drum sizes from 175 to 1000 litres is used for coating tablets with films and sugar.