2021/02/22

BionicSwift_new_4

The creation of the BionicSwift represents the next chapter for Festo in the development of bionic flying objects. As in its biological model, the use of lightweight structures is at the heart of the artificial bird. Because in both engineering and in nature, the less weight there is to move, the less material is required, and the less energy is consumed.

Foto (van webkwaliteit)

© Festo SE & Co. KG

Foto (van afdrukkwaliteit)

Trefwoorden