Operating costs for pneumatic equipment can be reduced by up to 60% if system operators put into practice the results and analyses of the Compressed Air Energy Efficiency Audit GFAA by Festo. Energy efficiency experts from Festo use an integrated approach to analyse the entire compressed air system, from the compressor to the application, and recommend measures to reduce energy consumption. Climate protection is also included in the service, since the cost and energy savings naturally result in lower CO2 emissions and higher productivity. Persbericht lezen Afbeelding Festo SE & Co. KG 2022/04/25 | Global How many users of compressed air know where the ... Operating costs for pneumatic equipment can be reduced by up to 60% if system operators put into ... Persbericht lezen
The decentralised pressure and vacuum generator PGVA from Festo is a compact complete solution for laboratory automation. It integrates compressor, air preparation including filter system, reservoir and electronic pressure and vacuum control in the smallest of spaces. Persbericht lezen Afbeelding Festo SE & Co. KG 2022/04/12 | Wereldwijd Multifunctional in the smallest of spaces The decentralised pressure and vacuum generator PGVA from Festo is a compact complete solution for ... Persbericht lezen
Leading industrial companies from the automotive, pharmaceutical and food industries have clear CO2 targets for their products. These require machine builders to make significant energy savings in new machine generations compared with previous machines. This is precisely why Festo offers an unrivalled solution in the global compressed air system market with its energy efficiency module MSE6-C2M. Persbericht lezen Afbeelding Festo SE & Co. KG 2020/06/17 | Global Meeting the CO2 specifications of industrial ... Leading industrial companies from the automotive, pharmaceutical and food industries have clear CO2 ... Persbericht lezen